2016-07-20 1:32 AM
I'using
I do some test with LwIP_HTTP_Server_Netconn_RTOS examples.
This example use: - LwIp Library - LCD interface with the framebuffer mappend on the SDRAM 0xC0000000 All works fine I can do my Log on the LCD and the scroll is fast. For my project I need to use the SDRAM 0xC0000000 as system ram. So I look at the FMC_SDRAM_DataMemory example. I did necessary modification into the LwIP_HTTP_Server_Netconn_RTOS example. I fix the LwIP RX/Tx buffer address. Note: I need to change also the MPU_Config to make the LwIp working. (to avoid memory exception) Below the new MPU_Config() function: //&sharpdefine USE_INTERNAL_RAM (disco config) static void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct; /* Disable the MPU */ HAL_MPU_Disable(); /* Configure the MPU attributes as WT for SRAM */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; &sharpifdef USE_INTERNAL_RAM MPU_InitStruct.BaseAddress = 0x20010000; MPU_InitStruct.Size = MPU_REGION_SIZE_256KB; &sharpelse MPU_InitStruct.BaseAddress = 0xC0000000; MPU_InitStruct.Size = MPU_REGION_SIZE_8MB &sharpendif MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; &sharpifdef USE_INTERNAL_RAM MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; &sharpelse MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; &sharpendif MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; &sharpifdef USE_INTERNAL_RAM MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; //Strongly ordered MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; &sharpelse MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; //Shared device MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; &sharpendif MPU_InitStruct.SubRegionDisable = 0x00; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enable the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); } After this modification all works fine but the LCD scroll is very slow. I have a thread that blink a led each 250ms and when the system scrolls the led remain fixed about 1 second I make some test an look into the code and the part of the code that slower the scroll is: Into lcd_log.c: LCD_LOG_PUTCHAR { ... &sharpifdef SKIP_THIS for(idx = LCD_CacheBuffer_xptr ; idx < XptrNUM; idx++) { LCD_CacheBuffer[LCD_CacheBuffer_yptr_bottom].line[LCD_CacheBuffer_xptr++] = ' '; } &sharpendif ... } and void LCD_LOG_UpdateDisplay (void) { ... for (cnt = 0 ; cnt < YWINDOW_SIZE ; cnt ++) { index = (cnt + ptr )% LCD_CACHE_DEPTH ; BSP_LCD_SetTextColor(LCD_CacheBuffer[index].color); BSP_LCD_DisplayStringAtLine ((cnt + YWINDOW_MIN), (uint8_t *)(LCD_CacheBuffer[index].line)); } ... } If I enable the define SKIP_THIS the scroll time is twice faster but always slow respect the LwIP_HTTP_Server_Netconn_RTOS without modifications. #!stm32-!heap-!sdram-!malloc