2018-02-10 04:36 PM
here is my conditional breakpoints settings
I took exercise as <apnt_230.pdf> did at page 11, 15) watchpoints: Conditional Breakpoints.
The application can use conditional breakpoints. Why I can't? I got a dialogue saying that My
target device dose not support conditional breakpoints!
Actually, I am using the STMF407 Discovery board as the
<apnt_230.pdf> using.
So, why?
Turvey.Clive.002
#conditional-breakpointsSolved! Go to Solution.
2018-02-11 01:21 AM
Finally, I found I forget to check the box of Read and Write.
Turvey.Clive.002
Don't tell Bob boys, I make a stupid mistake. ^ ^His notes is very helpful to get the uVision debugger working, and act like a professional.
2018-02-10 06:37 PM
Not really functionality I use. You might want to check the state of the SB12 solder bridge, and the specific version of the board and ST-LINK firmware. Bob Boys the author of the app note is an occasional visitor here, I will share the post.
2018-02-10 08:06 PM
SB12 is connected as default.
My ST-LINK firmware updated recently. Version: V2.J29.S0
Here is my KEIL IDE details:
2018-02-11 01:21 AM
Finally, I found I forget to check the box of Read and Write.
Turvey.Clive.002
Don't tell Bob boys, I make a stupid mistake. ^ ^His notes is very helpful to get the uVision debugger working, and act like a professional.
2018-02-13 10:35 AM
Hello
I noticed this and by the time I got to answer - you had already found the problem.
You are not the first to forget this - I think there are three others over the years.
So I updated the appnote a bit. It is now on the Keil website.
Bob
2018-02-20 11:35 AM
Hello
I updated Appnote 230 and it is now on www.keil.com::
http://www.keil.com/appnotes/docs/apnt_230.asp
You can adapt this document to many other ST boards.
There have been many improvements and additions to uVision since the last version of this document.
Event Recorder, ULINKplus Power Measurement, FreeRTOS support, ETM trace features and so on....
Thanks
Bob
San Jose, California