cancel
Showing results for 
Search instead for 
Did you mean: 

IWDG minimum reload in STM32L452

miguelvp
Associate

Hello community!

I'm working with the independent watchdog with a STM32L452 MCU in the Nucleo-L452RE board and I'm facing a problem trying to set low values in the reload register. When I try to set the reload register to values lower than 5 cycles (IWDG->RLR < 4), no matter the value of the prescaler register, the watchdog resets the system.

The clock used in the system is the HSI and it is configured to be the source of the sysclk.

My suspicion is, that as it is said for the status register for the VDD voltage domain, some LSI/Prescaler cycles are needed to take into account the refresh. But in the datasheet (DS11912 Rev 7, page 180) is specified that the minimum reload value is for RL = 0x000 and nothing is said in the device errata sheet (ES0388 Rev 8) as a limitation of the peripheral.

Am I doing something wrong or missing something? Thank you in advance.

I left the code that I'm executing to reproduce the error. It configures the HAL and the system clock. Then the IRQs are disabled and the LED of the board and IWDG are configured. If there is a reset from the watchdog, the LED is turned on and the execution ends

int main(void) {
 
  // reset of all peripherals, Initializes the Flash interface and the Systick
  HAL_Init();
 
  // configure the system clock
  SystemClock_Config();
 
  // disable IRQs
  __disable_irq();
 
  /* configure LED */
  // enable clock
  uint32_t temp;
  RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;
  (void) RCC->AHB2ENR;
 
  // set GPIO_PIN_5 from GPIOA
  GPIOA->OTYPER &= ~(0x1 << 5);
  GPIOA->PUPDR &= ~(0x3 << (5 * 2));
  temp = GPIOA->MODER;
  temp &= ~(0x3 << (5 * 2));
  temp |= (GPIO_MODE_OUTPUT_PP << (5 * 2));
  GPIOA->MODER = temp;
 
  // check reset cause and set led if iwdg reset
  if (RCC->CSR & (1 << RCC_CSR_IWDGRSTF_Pos)) {
    // clear reset cause
    RCC->CSR |= RCC_CSR_RMVF;
 
    // set LED
    GPIOA->BSRR = GPIO_PIN_5;
    while (1) {} // infinite wait
  }
 
  /* configure IWDG peripheral */
  // stop IWDG in debug
#ifdef DEBUG
  DBGMCU->APB1FZR1 |= DBGMCU_APB1FZR1_DBG_IWDG_STOP;
#endif
 
  // configure registers
  IWDG->KR = ((uint32_t)0x0000CCCC); // enable
  IWDG->KR = ((uint32_t)0x00005555); // enable register access
  IWDG->PR = ((uint32_t)0x00000006); // prescaler (no matter the value, but < 0x7)
  IWDG->RLR = ((uint32_t)0x00000003); // reload (>= 0x4 OK, < 0x4 NOK)
  while (IWDG->SR != 0x00u) {} // wait
 
  // infinite loop
  while (1) {
    IWDG->KR = ((uint32_t)0x0000AAAA); // feed
  }
}

1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

I don't use watchdogs nor the 'L4, but it reminded me of this https://community.st.com/s/feed/0D50X00009XkW4gSAF

JW

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

I don't use watchdogs nor the 'L4, but it reminded me of this https://community.st.com/s/feed/0D50X00009XkW4gSAF

JW

ATena.1
Associate

I can confirm that I am able to replicate this issue.

Yes, it seems to be the same problem that I am facing. Thanks a lot for the help

I didn't find the feed in my previous searches, sorry for the duplicate. I hope, at least, this will help other users in the future.

Thanks a lot again.

Miguel

CNien
Associate II

This also happens on my STM32C031 and it is really annoying that nothing is documented or that the HAL would prevent values lower than 4.