cancel
Showing results for 
Search instead for 
Did you mean: 

Issue receiving CAN Frames

Erwan03
Associate III

Hello ST community,

 

I am currently programming an ECU system, using f446re nucleo board. Right now i am trying to communicate with BMS using CAN communication.

So far, everything has been set: CAN Initialization and start, sending works properly.

The issue i am facing is that i cannot receive frames from battery, even though i can communicate with laptop for UDS protocole (Reception works properly in that case), but when i try with the battery, the debug mode doesn't stop at the rx interrupt routine.

I have verified the CANFilter configuration to make sure, i didn't see any mistake, nothing has been changed but i only can communicate with UDS frames and not with batteries.

for example: frame ID 0x586 entering fifo0 with such a filter:

 

void CAN_Filter_FIFO0(CAN_HandleTypeDef* hcan)

{

CAN_FilterTypeDef canfilterconfig;



canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;

canfilterconfig.FilterBank = 10;

canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;

canfilterconfig.FilterIdHigh = 0x580 << 5; // According to the DBC

canfilterconfig.FilterIdLow = 0x0000;

canfilterconfig.FilterMaskIdHigh = 0xfe0<<5;// Calculation of the mask according to the DBC

canfilterconfig.FilterMaskIdLow = 0x0000;

canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;

canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

canfilterconfig.SlaveStartFilterBank = 13;

HAL_CAN_ConfigFilter(hcan, &canfilterconfig);

}

Please let me know if anyone has any idea.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Erwan03
Associate III

Alright, found the problem, I was using both fifo0 and fifo1 for receiving whereas i had to use only one for all the frames. Don't know how to use both of them s

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
	HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxFrame);
	  {
		  switch(RxHeader.StdId)
		  {
		  	  case 0x586:
				  BatteryChargeCurrent_rcv(RxFrame, &rx_BCC); //Receive frame
				  BatteryChargeCurrent_memHandler(rx_BCC, &h_BCC); //handle memory
				  BCCFlag++;
				  break;
		  	case 0x591:
				  BatteryCurrentLimit_rcv(RxFrame, &rx_BCL); //Receive frame
				  BatteryCurrentLimit_memHandler(rx_BCL, h_BCL); //handle memory
				  BCLFlag++;
				  break;
			  case 0x587:
				  BatteryStatusCharge_rcv(RxFrame, &rx_BSC); //Receive frame
				  BatteryStatusCharge_memHandler(rx_BSC, h_BSC); //handle memory
				  BSCFlag++;
				  break;
			  case 0x580:
				  BatteryStatusGeneral_rcv(RxFrame, &rx_BSG); //Receive frame
				  BatteryStatusGeneral_memHandler(rx_BSG, h_BSG); //handle memory
				  BSGFlag++;
				  break;
			  case 0x59f:
				  BatteryVehicleHandling_rcv(RxFrame, &rx_BVH); //Receive frame
				  BatteryVehicleHandling_memHandler(rx_BVH, h_BVH); //handle memory
				  BVHFlag++;
				  break;
		  	  case 0x24:
		  		  EPIC_PMZ_A_rcv(RxFrame, &rx_pmzA); //Receive frame
		  		  EPIC_PMZ_A_memHandler(rx_pmzA, h_PMZ_A); //handle memory
		  		  break;
		  	  case 0x50:
		  		  EPIC_PMZ_C_rcv(RxFrame, &rx_pmzC); //Receive frame
		  		  EPIC_PMZ_C_memHandler(rx_pmzC, h_PMZ_C); //handle memory
		  		  break;
		  	  case 0x5A:
		  		  EPIC_PMZ_E_rcv(RxFrame, &rx_pmzE); //Receive frame
		  		  EPIC_PMZ_E_memHandler(rx_pmzE, h_PMZ_E); //handle memory
		  		  break;
		  	  case 0x5E:
		  		  EPIC_PMZ_G_rcv(RxFrame, &rx_pmzG); //Receive frame
		  		  EPIC_PMZ_G_memHandler(rx_pmzG, h_PMZ_G); //handle memory
		  		  break;
		  	  case 0x60:
		  		  EPIC_PMZ_H_rcv(RxFrame, &rx_pmzH); //Receive frame
		  		  EPIC_PMZ_H_memHandler(rx_pmzH, h_PMZ_H); //handle memory
		  		  break;
		  	  case 0x4e2:
		  		  EPIC_PMZ_I_rcv(RxFrame, &rx_pmzI); //Receive frame
		  		  EPIC_PMZ_I_memHandler(rx_pmzI, &h_PMZ_I); //handle memory
		  		  break;
		  	  case 0x621:
		  		  HMI_DATA1_rcv(RxFrame, &rx_cluster); //Receive frame
		  		  HMI_DATA1_memHandler(rx_cluster, h_HMI); //handle memory
		  		  break;
		  	  case 0x719:
		  		  UDS_DIAG_rcv(RxFrame);
		  		  UDSFlag ++;
		  		  break;
		  	  case 0x700:
		  		  DCDC700_rcv(RxFrame, &rx_dcdc700); //Receive frame
		  		  DCDC700_memHandler(rx_dcdc700, DCDC_700); //handle memory
		  		  break;
		  	  case 0x703:
		  		  DCDC703_rcv(RxFrame, &rx_dcdc703); //Receive frame
		  		  break;
		  	  default:
		  		  sprintf(msg, "Unknown ID in FIFO 1\r\n");
		  		  HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
		  		  break;
		  }
	  }
}

imultaneously. Then i used only one to receive the frames and it works.

Hello,

You can use them both simultaneously. According to the code source you shared at the beginning I don't see an issue.

For each FIFO you can set a filter config, so you will receive the matching message on that FIFO.

Maybe you didn't explain or provide more details of what you intended to do...

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.