2014-12-01 1:49 PM
I'm stuck on TIM triggered DMA to SPI.
My DMA Code configuration is as follow: void DMA_Configuration(void) { DMA_InitTypeDef DMA_InitStructure; /* Enable DMA1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* Blank DMA Configuration */ DMA_DeInit(DMA1_Channel1); /* Using the default values at Startup */ DMA_StructInit(&DMA_InitStructure); /*Changes from the default values */ DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(SPI2->DR); // Address of peripheral the DMA must map to => SPI2 Data Register DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t) TTxBuffer; // Variable to which received data will be stored DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; // Direction of transfer Memory to Peripheral =Destinatary DMA_InitStructure.DMA_BufferSize = 32; // BufferSize DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; // We don't want to change the SPI2 Data register DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; // We increment Memory DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; // We define Peripheral Data Size as Byte DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; // We define Memory Data Size as Byte DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; // Circular Mode define DMA_InitStructure.DMA_Priority = DMA_Priority_High; // High Priority DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; // Memory to Memory Disable /* Initialize the DMA */ DMA_Init(DMA1_Channel1, &DMA_InitStructure); /* Enable the DMA transfer half and complete interrupt */ DMA_ITConfig(DMA1_Channel1, DMA_IT_HT, ENABLE); // Half Transfer Interrupt Enable DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE); // Full transfer Interrupt Enable /* Enable the DMA TIM Triggered */ TIM_DMACmd(TIM2, TIM_DMA_Trigger, ENABLE); TIM_DMACmd(TIM2, TIM_DMA_Update, ENABLE); /* Enable DMA1 Channel1 */ DMA_Cmd(DMA1_Channel1, ENABLE); } Looking at DMA_CCR1 gives me 0x2AB7 which is ok. Looking at the SPI2_DR I found no value ; i.e. 0 Franck2014-12-12 9:03 AM
2014-12-12 9:35 AM
DMA_InitStructure.DMA_BufferSize = 2; // 2x 16-bit words, 1x 32-bit word, check endian/ordering
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; // The register is 16-bit wide
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
2014-12-15 12:51 AM
Hi Clive,
The greatest experience in life: Sharing knowledge! Thanks again Clive! Many thanks!2014-12-17 2:56 AM
Is there any way to add to that code a one pulse generation synchronized with TIM1?
I would like to have a pulse every 3.5*freq(TIM1)=delay and pulse time=0.5*Period(TIM1). I attached a figure of what is needed. Thanks in advance. ________________ Attachments : TIM2_pulse.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I16v&d=%2Fa%2F0X0000000biU%2FiIuaT4.99Yk2prcorjRg9s5qlslndEr2d84m4W7AjJ4&asPdf=false2014-12-17 6:03 AM
My unsuccessful added code:
/* Select the Master Slave Mode */TIM_SelectMasterSlaveMode(TIM1, TIM_MasterSlaveMode_Enable);
/* Master Mode selection */
TIM_SelectOutputTrigger(TIM1, TIM_TRGOSource_Update);
/* Slaves Configuration: PWM1 Mode */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = Period / 2;
TIM_OC1Init(TIM2 , &TIM_OCInitStructure);
/* Slave Mode selection: TIM2 */
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Gated);
TIM_SelectInputTrigger(TIM2, TIM_TS_ITR1); I have define TIM2 CH1 at PA0 of my nucleo board STM32F302R8T6 as follow: GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 ; // TIM2_CH1 (PA0)
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_1); // TIM2_CH1 PA0 AF1