cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a way to decode picture(1920 * 1080) within 50ms?

snkparty1
Associate III

We use STM32H743 to develop a system that needs to display a 1920 * 1080(8-bit pixel depths) graphic on LCD(driven by FPGA)

Now our design is that STM32 reads a picture from the SD card, then decodes and sends it to the FPGA through FMC.

We tried the software decoder, but it takes almost 5 seconds to decode just one PNG picture. The required time is only 50ms(about 3 FPS for each graphic, so 3*16ms = 48ms).  

I just learned that STM32H743  has an internal JPEG hardware decoder, but it seems this JPEG hardware decoder does not support 1920 * 1080? So the only way is to use an external decode chip, am I right?

0 REPLIES 0