cancel
Showing results for 
Search instead for 
Did you mean: 

Is the HAL libraries for CAN-bus the same for all STM32 microcontrollers?

DMårt
Lead

Hi!

I just have written a SAE J1939 library for CAN-bus. Yes it works.

But I got a request from someboy and he asking me if I could make this so it not only fit STM32F3 series. It need to fit all STM32 series.

https://github.com/DanielMartensson/Open-SAE-J1939

So my question is:

The HAL libraries in this code, is for STM32F3 series. But does it work with other STM32 series as well?

And one more question:

How large is the can bus buffer for reading a message?

I mean, the message will be stored inside the STM32 until I read it? Right?

How many CAN messages can an STM32 hold? 1 at the time? Or multiple messages in a queue?

/*
 * CAN.c
 *
 *  Created on: Jun 14, 2021
 *      Author: Daniel Mårtensson
 */
 
#include "Functions.h"
 
static CAN_HandleTypeDef *can_handler;
static uint32_t CAN_ID = 0;
static uint8_t RxData[8] = {0};
static bool new_message = false;
static void Create_CAN_Filter(CAN_HandleTypeDef *hcan);
static void Create_CAN_Interrupt(CAN_HandleTypeDef *hcan);
 
void STM32_PLC_Start_CAN(CAN_HandleTypeDef *hcan) {
	can_handler = hcan;
	Create_CAN_Filter(hcan);
	if (HAL_CAN_Start(hcan) != HAL_OK)
		Error_Handler();
	Create_CAN_Interrupt(hcan);
}
 
HAL_StatusTypeDef STM32_PLC_CAN_Transmit(uint8_t TxData[], CAN_TxHeaderTypeDef *TxHeader) {
	uint32_t TxMailbox;
	return HAL_CAN_AddTxMessage(can_handler, TxHeader, TxData, &TxMailbox);
}
 
/* Returns true if the message data is new */
void STM32_PLC_CAN_Get_ID_Data(uint32_t* ID, uint8_t data[], bool* is_new_message) {
	*ID = CAN_ID;
	memcpy(data, RxData, 8);
	*is_new_message = new_message;
	new_message = false;
}
 
/* Interrupt handler that read message */
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan) {
	CAN_RxHeaderTypeDef RxHeader;
	if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
		Error_Handler();
 
	/* Read ID */
	if(RxHeader.IDE == CAN_ID_STD){
		CAN_ID = RxHeader.StdId;
	}else{
		CAN_ID = RxHeader.ExtId;
	}
	new_message = true;
}
 
static void Create_CAN_Interrupt(CAN_HandleTypeDef *hcan) {
	if (HAL_CAN_ActivateNotification(hcan, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
			Error_Handler();
}
 
static void Create_CAN_Filter(CAN_HandleTypeDef *hcan) {
	CAN_FilterTypeDef sFilterConfig;
	sFilterConfig.FilterBank = 0;
	sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
	sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
	sFilterConfig.FilterIdHigh = 0x0000;
	sFilterConfig.FilterIdLow = 0x0000;
	sFilterConfig.FilterMaskIdHigh = 0x0000;
	sFilterConfig.FilterMaskIdLow = 0x0000;
	sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
	sFilterConfig.FilterActivation = ENABLE;
	sFilterConfig.SlaveStartFilterBank = 14;
 
	if (HAL_CAN_ConfigFilter(hcan, &sFilterConfig) != HAL_OK)
		Error_Handler();
}

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0