cancel
Showing results for 
Search instead for 
Did you mean: 

Is it necessary to test both IWDG and WWDG for IEC 60335-1 class B compliance?

Anitha
Associate III

The ST self-test library(en.x-cube-classb-v2-3-0) tested both watchdogs( IWDG and WWDG). Is it necessary to test both IWDG and WWDG for class B compliance? In the self-test library, they used both watchdogs. If I use one watchdog timer let's say WWDG then Do I need to test other one(IWDG) for class B compliance?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0