2008-11-28 4:15 AM
Interrupts: level / edge
2011-05-17 3:54 AM
I've a interrupt input that's low while there's data for me, not an uncommon mode. The only config option I can find in the micro is for rising, falling or both edges. Is there not a ''level'' mode such that on exiting the IRQ handler the core re-detects the ''level'' and repeats until the data has been dealt with? Do I have to poll the input within the IRQ handler, moving data until it's negated?
The ARM manual (http://infocenter.arm.com/help/topic/com.arm.doc.ddi0337e/DDI0337E_cortex_m3_r1p1_trm.pdf) for the NVIC mentions ''Level vs pulse'' that looks just the ticket, but there's no mention in the ST blurb. Anyone any ideas? Also, what's the difference between a port pin interrupt and event?2011-05-17 3:54 AM
one solution is to set the pending bit of the irq at the end of the isr:
irq_pending_bit = ! irq_level It is only one instruction and everything should work.