cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt Problems

ezrab
Associate II
Posted on October 12, 2010 at 17:08

hi

i have aquestion about Interrupts:

in all the example code that i saw i could never find where the program goes to in case of an Interrupt.

here is one of the exmple code i have from st site which the button activate external Interrupt but where does the program goes in that case??

/**

  ******************************************************************************

  * @file    EXTI/main.c

  * @author  MCD Application Team

  * @version V3.3.0

  * @date    04/16/2010

  * @brief   Main program body

  ******************************************************************************

  * @copy

  *

  * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS

  * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE

  * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY

  * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING

  * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE

  * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS.

  *

  * <h2><center>&copy; COPYRIGHT 2010 STMicroelectronics</center></h2>

  */

/* Includes ------------------------------------------------------------------*/

#include ''stm32f10x.h''

#include ''stm32_eval.h''

/** @addtogroup STM32F10x_StdPeriph_Examples

  * @{

  */

/** @addtogroup EXTI_Example

  * @{

  */

/* Private typedef -----------------------------------------------------------*/

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

/* Private function prototypes -----------------------------------------------*/

/* Private functions ---------------------------------------------------------*/

/**

  * @brief  Main program.

  * @param  None

  * @retval None

  */

int main(void)

{

  /*!< At this stage the microcontroller clock setting is already configured,

       this is done through SystemInit() function which is called from startup

       file (startup_stm32f10x_xx.s) before to branch to application main.

       To reconfigure the default setting of SystemInit() function, refer to

       system_stm32f10x.c file

     */    

        

  /* Initialize LED1 and Key Button mounted on STM3210X-EVAL board */      

  STM_EVAL_LEDInit(LED1);

  STM_EVAL_PBInit(BUTTON_KEY, BUTTON_MODE_EXTI); 

  /* Generate software interrupt: simulate a falling edge applied on Key Button EXTI line */

  EXTI_GenerateSWInterrupt(KEY_BUTTON_EXTI_LINE);

       

  while (1)

  {

  }

}

#ifdef  USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *         where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

/**

  * @}

  */

/**

  * @}

  */

/******************* (C) COPYRIGHT 2010 STMicroelectronics *****END OF FILE****/

thanks...

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 12, 2010 at 18:16

i have aquestion about Interrupts:

 

in all the example code that i saw i could never find where the program goes to in case of an Interrupt.

 

 

here is one of the exmple code i have from st site which the button activate external Interrupt but where does the program goes in that case??

 

Typically the interrupt routines are in the file stm32f10x_it.c within the project.

/**

  * @brief  This function handles External line0 interrupt request.

  * @param  None

  * @retval None

  */

void EXTI0_IRQHandler(void)

{

  if(EXTI_GetITStatus(USER_BUTTON_EXTI_LINE) != RESET)

  {

    /* Toggle LED3 */

     STM32vldiscovery_LEDToggle(LED3);

    /* Clear the User Button EXTI line pending bit */

    EXTI_ClearITPendingBit(USER_BUTTON_EXTI_LINE);

  }

}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..