2016-01-28 1:00 PM
2016-01-28 10:48 PM
I resolved a couple of issues which were affecting this problem and I wanted to follow up for anyone who comes upon this thread.
After logging the transmit descriptor status word value I discovered that collisions were occurring when packets were being dropped and that re-transmit was disabled. Enabling re-transmit fixed the problem.In addition I found that the the PHY_SR define in stm32_eth.h (from some reference source code) is PHY specific. It was incorrect for the PHY I am using, so the duplex state was incorrect (thought it was half duplex, when in fact it was full duplex). I just had to update the register, PHY_Speed_Status, and PHY_Duplex_Status defines to match that of the LAN8720A.Best regards,Element