Installing ST-LINK/V2 USB drivers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 1:57 PM
Hi, I'm a newbie, and I have just started working with STM32 and the GNU tools available, and can anybody explain what is correct from the following quote on how to install
which is on (http://gnuarmeclipse.github.io/openocd/install/
) OpenOcd: ST-LINK/V2One example of compatible drivers are the ST-LINK/V2 USB drivers, from ST, available as part number
http://www.st.com/web/en/catalog/tools/FM147/SC1887/PF260219
. Download thestsw-linkzip
archive, extract its content to a separate folder, and run the
dpinst_amdexe
(or
dpinst_xexe
) with administrative privileges.
I Have two versions of OpenOCD
ST-LINK_USB_V2_1_Driver
and
ST-LINK_USB_V2_Driver
Has anyone done it this way before?
Thanks.
#openocd
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 2:43 PM
I'm not even sure what the question is. I don't know what version of Windows you have, or what specific ST-LINK you have.
The V2.1 drivers are for the mbed enabled version of the ST-LINK I'd start by using the ST-LINK Utilities, make sure you update the firmware, and then use the V2 or V2.1 driver package as appropriate, and the 32-bit or 64-bit installer depending on your version of Windows. I suspect the V2.1 stuff will also work with the older V2. I pretty much use the ST-LINK, DISCO, and NUCLEO boards interchangeably and really don't have a lot of issues with the drivers.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-08 6:27 PM
Hi Clive1. I have Windows10, and I use the older stm32vldiscovery board, and I also have a Olimex P103. I program my P103 using an St-Link/V2, and the discovery with the built in programmer that comes with the unit, as you would already know.
I have my eclipse IDE working at the moment as far as editing compiling and programming, but I want to set up the debugger. So far I have installed OpenOCD, but I'm a bit confused about runningdpinst_amd64.exe, arnt the drivers already installed? and do I also have to install QEMU? is this just a simulator? or also a on chip debugger?
Thanks Clive cheers