Skip to main content
Clonimus74
Senior II
June 24, 2018
Question

Inspecting registers in IAR EWARM 8.22

  • June 24, 2018
  • 2 replies
  • 1097 views
Posted on June 24, 2018 at 11:17

Hi all,

I hope someone here can help.

When I debug my application (STM32L476QE) using IAR embedded workbench V8.22, I try to watch the NVIC registers

(View->Registers-> Rigisters 1, then right click and selecting 'View Group->Nested Vectored Interrupt Controller'), but all of their values are seen as 0x00000000 (even though that is not the actual value for sure).

What can be the problem?

The mapping of the resters within IAR are correct as seen in 'Project->SFR Setup'.

#iar-ewarm
This topic has been closed for replies.

2 replies

Clonimus74
Senior II
June 26, 2018
Posted on June 26, 2018 at 11:08

No one encountered this?

Tesla DeLorean
Guru
June 26, 2018
Posted on June 26, 2018 at 14:58

>>No one encountered this? 

The lack of response suggest a lack of constituency, right?

Perhaps try working with IAR Support

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..