2025-12-30 5:13 PM
Hello,
I am currently working with the LSM6DSOX sensor in an I3C-based system on STM32 and would like to inquire if there is a Linux driver or example code available for I3C slave mode with In-Band Interrupt (IBI) support.
My goal is to implement the I3C slave functionality in a Linux environment, where I can utilize IBIs for efficient communication. Could you please provide information on the following:
- Is there any existing Linux driver or example for I3C slave mode with IBI support for LSM6DSOX?