cancel
Showing results for 
Search instead for 
Did you mean: 

In STM32L562VET6Q Microcontroller in that my question is how to configure/map SRAM 2 memory address as 0x2003 0000, so , i can use it as contiguous memory of both SRAM 1 and SRAM 2 i need big size continuous memory block.

sra
Associate II

"64 Kbytes located at address 0x0A03 0000 with hardware parity check (SRAM2). This memory is also mapped at address 0x2003 0000 offering a contiguous address space with the SRAM1"

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bubbles
ST Employee

Hi @sra​ ,

look at the memory map figure in the reference manual (chapter 2.3.2).

The same physical memory is accessed on different address ranges depending on the access type. Non-secure or non-secure callable for code, non-secure or secure if data.

If the TZ on your device is disabled or configured to have the SRAM2 non-secure, you should be able to access the SRAM2 at 0x2003 0000.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.