cancel
Showing results for 
Search instead for 
Did you mean: 

In STM32F0x1, for internal temperature sensor sampling time must be greater than 4 uSec that means at 48 MHz only one option Sampling time 239.5 ADC clock cycles.

DTriv
Associate

STM32F0x1 do not support different sampling time for different channel, what should be the configuration if i want to sample other external ADC signal with high sampling frequency with Sampling time 1.5 ADC clock cycle.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AvaTar
Lead

Use a device with two ADC peripherals, or skip the temperature channel entirely.

The chip die temperature is not really of much use in most cases.

Or add a cheap external sensing element. With proper calibration, a simple PN junction (diode) in formward direction will do.