Implement a usart1 receive interrupt without pressing a key
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-01 12:28 AM
Hello Forum,
I have implemented a menu system on my app using the console
Main Menu Select A ....1 (e.g. prints Debug1)
Main Menu Select B.....2 2 Sub Menu B Select A ......1 Sub Menu B Select B.......2 1 Carry out Sub Menu B Select A action....e.g print debug2 Sub Menu B Select A ......1 Sub Menu B Select B.......2 1
After selecting Main menu B by pressing '2', I enter the sub menu from which I can select any of the sub menu options. Aften completing the sub menu action, I redisplay the sub menu to give the user the opportunity to select from it again if required. However when I press '1 ' again it takes me back into main menu '1' action where it prints Debug1. I can understand this as the usart interrupt just sees a '1' . However I want it to carry out the sub menu action.
After completing the sub menu action I think I need to make the usart1 receive interrupt think that a '2' has been pressed so that it resisplays the sub menu again. I tried the following but it doesn't seem to work.
char sub_menu_option = '2';
scanf(''%c'', &sub_menu_option);Is there a way to do this or is this nonsense and is there an easier way?
Apologies if this is very convoluted but any help would be greatly appreciated.
Dave
#!psychic #stm32 #state-machine #fsm- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-01 5:48 AM
Perhaps you want to look at the implementation more carefully. Use routines like getchar() or there equivalents, and check if scanf() is returning -1 before using the values returned.
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
‎2014-09-01 5:55 AM
''the usart interrupt just sees a '1'''
Doing it in the ISR may well not be a good idea - but that's a separate issue.If you want the ISR to be able to handle a '1' differently depending on which menu is currently displayed then, clearly, your ISR will have to be aware of which menu is currently displayed!In other words, the ISR needs a notion of state.So a good technique could be a State Machine - aka Finite State Machine (FSM), or Finite State Automaton (plural: Automata)
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-01 11:45 PM
Hi Guys,
Thanks for assisting. I'm implementing it as a state machine now, so it looks to be working OK now. It is probably is a bit safer than messing with the stack frame. Dave.