cancel
Showing results for 
Search instead for 
Did you mean: 

IEC60335 SelfTestLib

SomeDeveloper
Associate II

In our legacy STM32f103 project a ST library named "Self Test Library" is used. It has version 1.0, dated 10/01/2007. That library is certified according to IEC60335. I found it in an archive named IEC60335.zip, but I have no idea if that's the original archive name. Source files are named "stm32f10x_STL*.h/.c.

Is the library still maintained? 

Can the original archive be downloaded somewhere?

Are newer versions available?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0