IEC60335 SelfTestLib
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-23 6:11 AM
In our legacy STM32f103 project a ST library named "Self Test Library" is used. It has version 1.0, dated 10/01/2007. That library is certified according to IEC60335. I found it in an archive named IEC60335.zip, but I have no idea if that's the original archive name. Source files are named "stm32f10x_STL*.h/.c.
Is the library still maintained?
Can the original archive be downloaded somewhere?
Are newer versions available?
Labels:
- Labels:
-
STM32F1 Series
0 REPLIES 0