2008-01-31 11:56 PM
IAR STM32-SK evaluation board example
2011-05-17 03:22 AM
Hi Becheur !
Try downloading the ARM-based 32-bit MCU STM32F101xx and STM32F103xx firmware library zip & pdf files here: Look in the firmware section. USART example # 7 retargets the C library printf function to the USART. Should be able to port over to the IAR toolchain & IAR SK dev board. I will be working on this next week.2011-05-17 03:22 AM
Hello everybody,
is there anyone who can provide me an IAR project environment to send a simple printf'''' through RS232_2 port on the STM32-SK IAR version board? thank you !!