cancel
Showing results for 
Search instead for 
Did you mean: 

I2S passthrough - but STM32 only has one I2S data pin ?

freeflyer
Senior II

I am developing I2S on the NUCLEO-L433RC-P development board using a BT401 bluetooth audio receiver and MAX98357A I2S amplifier.

I need to pass the I2S audio data through the STM32L4333 (refer to diagram below). 

I have done this before using a Microchip dsPIC33E but this has both DATA IN and DATA OUT pins for I2S.

Whereas the STM32 only has a single DATA pin (SD), so it can only be DATA IN or DATA OUT.

Does this mean I cannot use the STM32 to pass through I2S data ?

freeflyer_0-1764239514938.png

 

0 REPLIES 0