2009-03-06 6:26 AM
I2S DMA
2011-05-17 4:05 AM
Hello,
I have been strugling on getting DMA to I2S on SPI3 to work... I can't get it to work in the primer2 or in the keil simulator, i am not sure how the simualtor shows DMA transfers, or if it is not capable of that. here is my code, can anyone see some errors?Code:
DMA_InitTypeDef DMA_InitStructure; I2S_InitTypeDef I2S_InitStructure; u16 kj[] = {1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16}; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); RCC_APB1PeriphClockCmd( RCC_APB1Periph_SPI3 , ENABLE); I2S_Cmd(SPI3, DISABLE); I2S_InitStructure.I2S_Standard = I2S_Standard_MSB; I2S_InitStructure.I2S_DataFormat = I2S_DataFormat_16b; I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Disable; I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_44k; I2S_InitStructure.I2S_CPOL = I2S_CPOL_Low; I2S_InitStructure.I2S_Mode = I2S_Mode_MasterTx; I2S_Init(SPI3, &I2S_InitStructure); SPI_I2S_DMACmd(SPI3, SPI_I2S_DMAReq_Tx, ENABLE); I2S_Cmd(SPI3, ENABLE); /* DMA1 Channel7 configuration ----------------------------------------------*/ DMA_DeInit(DMA1_Channel7); DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)&SPI3->DR;//0x40003c0c; // SPI3 Data register DMA_InitStructure.DMA_MemoryBaseAddr = (u32)&kj; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 15; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; // WORD?? DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel7, &DMA_InitStructure); DMA_ITConfig(DMA1_Channel7, DMA_IT_TC|DMA_IT_HT, ENABLE); DMA_Cmd(DMA1_Channel7, ENABLE); Br Kasper (pst. I will possible post this on the STM32Circle forum as well)