2025-01-21 11:32 PM
Hello, this is DK.
I am working on a project using stm32f429IIt6.
I'm currently having an I2C problem at the end of my project.
I2C1 uses PF 0, 1 / I2C2 uses PB 6, 7. The HW PCB completed, and the HW I2C pull up is the same.
In I2C1 HAL code, the entire initialization does not work, and if I2C2 is used with the same code, it works well.
I am using various Pheripherals such as TIM Interrupt. Is there any conflict?
Is there any difference between I2C1 and I2C2?
In the TIMER part, it appears to share APB1.