2008-05-06 3:01 AM
I2C STOP SDA does not go back to high level
2011-05-17 3:34 AM
Hello,
I'm using the um0427 library, and after a stop the SCL is at the high level, but the SDA not go back to high level, On the scope trace we can also see the glitchs already evoked (http://www.st.com/mcu/forums-cat-6701-23.html) gpio/i2c config ******* /* Configure I2C1 pins: SCL and SDA ------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_Init(GPIOB, &GPIO_InitStructure); /* I2C1 configuration ---*/ I2C_DeInit(I2C1); I2C_InitStructure_1wire.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure_1wire.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure_1wire.I2C_OwnAddress1 = I2C1_SLAVE_ADDRESS7; I2C_InitStructure_1wire.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure_1wire.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure_1wire.I2C_ClockSpeed = 50000; I2C_Init(I2C1, &I2C_InitStructure_1wire); /*---------------*/ code ************************* void resetds2482(void){ /* Send I2C1 START condition */ I2C_GenerateSTART(I2C1, ENABLE); /* Test on I2C1 EV5 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, DS2482, I2C_Direction_Transmitter); /* Test on I2C1 EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); /* Envoi du Reset */ I2C_SendData(I2C1, DRST); /* Test on I2C1 EV8 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); /*Si la commande a réeussi le 2482 répond par un octet on Restrart l'I2C en Reception*/ I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, DS2482, I2C_Direction_Receiver); /* Test on EV6 and clear it */ while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); /*Recuperation du Status Registger ---*/ regvalue = I2C_ReceiveData(I2C1); while(I2C_GetFlagStatus(I2C1, I2C_FLAG_RXNE)); /* Send I2C1 STOP Condition */ I2C_GenerateSTOP(I2C1, ENABLE); GPIOB->BSRR = GPIO_Pin_7; myDelay(80000); } [ This message was edited by: julien.massot on 06-05-2008 12:24 ] [ This message was edited by: julien.massot on 06-05-2008 12:26 ]2011-05-17 3:34 AM
Did you check my post (http://www.st.com/mcu/forums-cat-6701-23.html) ?
2011-05-17 3:34 AM
it's seems that it's the restart who cause this problems, how can i do a restart whithout stop ?
2011-05-17 3:34 AM
Hi,
Scope pictures are great! Have not used I2C on STM32 yet but have with other ARM. Check that you have proper pull-up R on SDA line AND that ''no other'' device on your I2C bus is pulling SDA down. Good luck.2011-05-17 3:34 AM
It's a Cortex M3 from ST (STM32f103),
The problem is that the acknoledge must be disable for the last byte reveived , i corrected it and it's works..