2008-08-26 3:06 AM
TIM3 input capture mode problem!
2011-05-17 3:34 AM
Hello!
i try to use the input capture function of timer3. summary: timer 3 is used as an up/down counter. channel 1 + 2 are used to create pwm signals on output pins. channel 3 should indicate rising edges of an input signal and should store the timer value in CCR3 register. initialization of channel 3:Code:
TIM_ICInitStructure.TIM_ICMode = TIM_ICMode_ICAP; TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM3, &TIM_ICInitStructure); enabled ITs:Code:
// TIM IT enable TIM_ITConfig(TIM3,TIM_IT_CC1, ENABLE); TIM_ITConfig(TIM3,TIM_IT_CC2, ENABLE); TIM_ITConfig(TIM3,TIM_IT_CC3, ENABLE); TIM_ITConfig(TIM3,TIM_IT_Update, ENABLE); The problem is that when Channel 3 is configured like described above, the channel 1 stops outputting PWM signals. how could i solve this problem???2011-05-17 3:34 AM
2011-05-17 3:34 AM
I am getting this problem too only with Timer 2. Have you worked out a solution yet?
2011-05-17 3:34 AM
There was an error in the firmware!
stm32f10x_tim.c function TI3_Config(TIM_TypeDef * ....... line 2431 is: tmpccer &= CCER_CC1P_Mask & CCER_CC1E_Mask; and should be: tmpccer &= CCER_CC3P_Mask & CCER_CC3E_Mask; #define CCER_CC3E_Mask ((u16)0xFEFF) is also missing! [ This message was edited by: m.taisser on 26-08-2008 14:13 ]2011-05-17 3:34 AM
Thanks,
I looked at the library code and my TIx_Config functions look reasonable. I then went to look at the PWMI_Config function and from what I deduced it seems to need Channel 1 or 2. So I change my code to output my signal on Channel 3: PWM_TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; PWM_TIM_OCInitStructure.TIM_Channel = TIM_Channel_3; PWM_TIM_OCInitStructure.TIM_Pulse = 250; PWM_TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInit(TIM2, &PWM_TIM_OCInitStructure); And to input PWM on Channel 1: TIM_ICStructInit(&PWM_TIM_ICInitStructure); PWM_TIM_ICInitStructure.TIM_ICMode = TIM_ICMode_PWMI; PWM_TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; PWM_TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; PWM_TIM_ICInitStructure.TIM_ICSelection=TIM_ICSelection_DirectTI; PWM_TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; PWM_TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM2, &PWM_TIM_ICInitStructure); And I now still see my PWM signal (On Pin PA2) Adam