2010-11-11 11:07 PM
I2C communication
2011-05-17 5:14 AM
Please provide the make/part number of the slave device, and the code you are using to initialize and communicate with the I2C bus.
2011-05-17 5:14 AM
2011-05-17 5:14 AM
It is STM32L152
NO THE SLAVE DEVICE If you aren't using the correct address, the I2C is not correctly initialized, or the part is simply not wired correctly, then the SLAVE device will NOT respond, there will be NO ACKNOWLEDGEMENT FOR IT.