cancel
Showing results for 
Search instead for 
Did you mean: 

I2C communication with X9258

mikeschultz9
Associate
Posted on September 30, 2011 at 10:17

Hello,

I've got a problem communicating with a X9258 poti via I2C. This Poti has a protocol like:

Start, Adress, send Byte, read two Bytes, Stop

so is it possible with the build in I2C hardware to switch between tranmitting and recieving without sending a second start?

Regards,

 Mike
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on September 30, 2011 at 11:37

''a X9258 poti''

 

 

You mean this:

http://www.intersil.com/data/fn/fn8168.pdf

 

?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.