2022-11-20 7:47 AM
I understand that there are many sensors available on B-L4S5I-IOT01A . But I am not able to find any tutorials or sample code for reading data from these sensors. If there is anything can anyone in this group help me
2022-11-20 12:38 PM
The firmware package (stm32cubel4) contains some demos. Check %USERPROFILE%\STM32Cube\Repository\ (Windows) and the STM32Cube_FW_L4_V1.17.2\Projects folder.
This is also avail. online on github: https://github.com/STMicroelectronics/STM32CubeL4.git
For your board is only a WiFi demo app showing temp.sensor on a web page. This demo uses the Board support Package (BSP) drivers, and there are more BSP drivers for various sensor available. See STM32Cube_FW_L4_V1.17.2\Drivers\BSP\B-L4S5I-IOT01
hth
KnarfB
2022-11-20 12:54 PM
Hello @GirishKumar and welcome to the Community :)
You will find various applications and you can get inspired from them to use sensors mounted on the B-L4-IOT boards.
The examples are available in the \Projects\B-L475E-IOT01A\Applications\ and run on STM32L475xx devices.
STM32CubeL4/Projects at master · STMicroelectronics/STM32CubeL4 · GitHub
If you are satisfied of my answer, please mark it as "Best", so that this thread will be marked as solved.
Imen
2022-11-21 4:14 AM
Hi Imen
Thanks for you response. I went to the folder what you had recommended I see only two applications NFC and WiFi or board I am using (B-L4S5I-IOT01A)
For B-L475E-IOT01A: I find one or two more examples
Proximity Sensor and Sub_Ghz in addition to NFC and Wifi
There is a temperature sensor, barometric pressure sensor, Accelrometer etc. I do not see sample code or examples for the these sensor. Is there way I can look for equivalent code for some other board I Can use it for (B-L4S5I-IOT01A)
It is bit urgent for project I am working.
I am trying to develop application which access these sensors on Azure RTOS.
Regards
Girish
2022-11-21 4:14 AM
Thanks for you response. I went to the folder what you had recommended I see only two applications NFC and WiFi or board I am using (B-L4S5I-IOT01A)
For B-L475E-IOT01A: I find one or two more examples
Proximity Sensor and Sub_Ghz in addition to NFC and Wifi
There is a temperature sensor, barometric pressure sensor, Accelrometer etc. I do not see sample code or examples for the these sensor. Is there way I can look for equivalent code for some other board I Can use it for (B-L4S5I-IOT01A)
It is bit urgent for project I am working.
I am trying to develop application which access these sensors on Azure RTOS.
Regards
Girish
2022-11-21 5:48 AM
That's why I said STM32Cube_FW_L4_V1.17.2\Drivers\BSP\B-L4S5I-IOT01 which contains easy-to-use APIs for those.
hth
KnarfB
2022-11-21 6:00 AM
Thanks a lot, these are the examples I was looking for.
Actually, I never expected these examples to be stored under BSP folder. That is why I could not connect earlier.
Once again Thanks for your help and support
Regards
Girish