2022-06-17 3:07 PM
I would need assistance in editing the linker script and the startup (.s) file to access the memory area from a c routine...
2022-06-26 11:48 AM
After a week of hair pulling, I finally solved it: For those trying to get the DAC2 on STMH7A chips. This is the secret:
In the linker script the SRD ram is listed. It is 32k in Length which should suit most DAC applications.
MEMORY
{
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
DTCMRAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
DTCMRAM2 (xrw) : ORIGIN = 0x20010000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
RAM_CD (xrw) : ORIGIN = 0x30000000, LENGTH = 128K
RAM_SRD (xrw) : ORIGIN = 0x38000000, LENGTH = 32K
}
So you need a definition of this memory area in the script in order to define it in gcc:
.DATA_RAM_SRD (NOLOAD) :
{
} >RAM_SRDIn your C file:
uint16_t m_array[ARR_LEN] __attribute__((section(".DATA_RAM_SRD")));Hey presto. DAC2 will behave like DAC1 (with 1 channel only). From what I can see it has the same specs as DAC2 except no FIFO and it can only synchronise with peripherals in the D3 domain (RCC Clock etc)