cancel
Showing results for 
Search instead for 
Did you mean: 

I have win7, just installed the Unicleo-Gui to Nucleo-F401RE

temo castro
Associate
Posted on September 26, 2017 at 00:07

My problem is Unicleo cant see any port, why?

STM32 ST-LINK Utility works perfectly, I can download/upgrade firmware but no success to Unicleo-Gui

Do I need to install something else?

1 ACCEPTED SOLUTION

Accepted Solutions
temo castro
Associate
Posted on September 27, 2017 at 15:54

Is working now, what I did it to load the hex file for

X-NUCLEO-IKS01A2 Acceleration calibration and after that it communicates, it seems the out-of-the-shelve F401RE comes with a program that doesn't communicate with Unicleo

View solution in original post

2 REPLIES 2
temo castro
Associate
Posted on September 27, 2017 at 15:54

Is working now, what I did it to load the hex file for

X-NUCLEO-IKS01A2 Acceleration calibration and after that it communicates, it seems the out-of-the-shelve F401RE comes with a program that doesn't communicate with Unicleo

Posted on January 06, 2018 at 21:11

I see this same problem, and your solution fixed it for me. They should update the docs to reflect this. Thanks!