cancel
Showing results for 
Search instead for 
Did you mean: 

I had some issues with USART3 with nucleo-H723. The board's UART3 is connected to st-linkV3,When I using USART3 to send data in keil, it works fine,but when I use Clion is, the PC serial port shows packet loss, and I want to know what is the reason an

chuan
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal

Well run a test sending continuously a text and user teraterm type app to check if any missing/skipped data. If not, the issue is probaby in CLion side, which you should send a post to the related community site.