cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32L053R8 Nucleo board. Is it possible to migrate X-CUBE-SMCARD firmware (AN4800) to work on my board (there is an example for STM32L0538DISCOVERY) without ST8024? I tried and at the moment I don't get any response from smart card.

ASavi.3
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bubbles
ST Employee

Yes, the readme file in the example project and the AN4800 should provide enough information on that. If the card in not sending an ATR, check what kind of card it is and if it works in a regular reader.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.