cancel
Showing results for 
Search instead for 
Did you mean: 

i am trying to read two timers frequency count and store in DMA , here i have configured two timers in TIM2_CH1, TIM5_CH2 in the input capture direct mode. i used HAL_TIM_IC_Start_DMA() functions to get frequency into DMA , Am in correct a approach ?

NPULI.1
Associate II

i am trying to read two timers frequency count and store in DMA , here i have configured two timers in TIM2_CH1, TIM5_CH2 in the input capture direct mode. i used HAL_TIM_IC_Start_DMA() functions to get frequency into DMA . is it correct approach .

i thought when we configure HAL_TIM_IC_Start_DMA() the Channel count wil store in DMA, but in some STM32 examples i saw few of are doing capture and compare and difference why we need this , when we configure in HAL_TIM_IC_Start_DMA() we get directly get into DMA and we will read back whenever required . i am searching on this from last one month still i didn't clarity . if one help it would be great please see my code and suggest me.

The frequency count and store in DMA for every 1sec using systic timer 

=====================================================================

TIM2_CH1, TIM5_CH4 :32 bit Timers

The TIM2, TIM5 intilized in input capture direct mode configured as acounter mode start counting the frequency

volatile uint32_t uFrequency1=0,uFrequency2=0;

volatile uint32_t vuPreviousFreqCnt1 = 0,vuPreviousFreqCnt2 = 0;

uint8_t uFREQUENCY_INPUT_1, uFREQUENCY_INPUT_2;

uint32_t ret =0;

uint32_t ucapture_count1[IC_BufSize] = {0x00000000}; // DMA buffer of CH1 used to store rising edge capture data

uint32_t ucapture_count2[IC_BufSize] = {0x00000000}; // DMA buffer of CH1 used to store rising edge capture data

extern TIM_HandleTypeDef htim2;

extern TIM_HandleTypeDef htim5;

extern DMA_HandleTypeDef hdma_tim2_ch1;

extern DMA_HandleTypeDef hdma_tim5_ch4_trig;

int main ()

{

 SystemClock_Config();

 MX_GPIO_Init();

 MX_TIM2_Init();

 MX_TIM5_Init();

 FrqCnt_init();

return (0);

}

/*Getting the frquency count */

void FrqCnt_init()

{

  if(HAL_TIM_IC_Start_DMA(&htim2, TIM_CHANNEL_1, (uint32_t *)ucapture_count1, IC_BufSize) != HAL_OK); // Get the T2 frquency count input capture mode

  {

   /* Error Code */

    Diag_SetErrorCode(ERROR_CODE_FI_ERR);

  }

  htim2.State = HAL_TIM_STATE_READY;

  if(HAL_TIM_IC_Start_DMA(&htim5, TIM_CHANNEL_4, (uint32_t *)ucapture_count2, IC_BufSize) != HAL_OK);// Get the T5 frquency count input capture mode

  {

   /* Error Code */

   Diag_SetErrorCode(ERROR_CODE_FI_ERR);

  }

}

/*frquency Deintlize fun */

void Freq_DeInit(void)

{

  HAL_TIM_IC_Stop_DMA(&htim2, TIM_CHANNEL_1);

  HAL_TIM_IC_Stop_DMA(&htim5, TIM_CHANNEL_4);

}

/* TIM2 init function */

void MX_TIM2_Init(void) 

{

 TIM_IC_InitTypeDef sConfigIC;

 htim2.Instance = TIM2;

 htim2.Init.Prescaler = 0;

 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim2.Init.Period = 0xffffffff;

 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 HAL_TIM_IC_Init(&htim2);

 htim2.Instance->CR1 &= ~(1<<0);   //clear counter register 

 htim2.Instance->CNT = 0; //initialy counter zero

 htim2.Instance->EGR = 0; //Update event can be generated at each counter overflow desabled

  

 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;

 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;

 sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;

 sConfigIC.ICFilter = 0;

 HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1);

}

/* TIM5 init function */

void MX_TIM5_Init(void) 

{

 TIM_IC_InitTypeDef sConfigIC;

 htim5.Instance = TIM5;

 htim5.Init.Prescaler = 0;

 htim5.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim5.Init.Period = 0xffffffff;

 htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 HAL_TIM_IC_Init(&htim5);

 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;

 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;

 sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;

 sConfigIC.ICFilter = 0;

 HAL_TIM_IC_ConfigChannel(&htim5, &sConfigIC, TIM_CHANNEL_4);

}

void HAL_TIM_IC_MspInit(TIM_HandleTypeDef* htim_ic)

{

  GPIO_InitTypeDef GPIO_InitStruct;

 if (htim_ic->Instance == TIM2) {

  /* Peripheral clock enable */

  __TIM2_CLK_ENABLE();

  /**TIM2 GPIO Configuration

   PA5   ------> TIM2_CH1

   */

  GPIO_InitStruct.Pin = GPIO_PIN_6;

  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

 //  GPIO_InitStruct.Alternate = GPIO_AF2_TIM2;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /* Peripheral DMA init*/

  hdma_tim2_ch1.Instance = DMA1_Stream5;

  hdma_tim2_ch1.Init.Channel = DMA_CHANNEL_3;

  hdma_tim2_ch1.Init.Direction = DMA_PERIPH_TO_MEMORY;

  hdma_tim2_ch1.Init.PeriphInc = DMA_PINC_DISABLE;

  hdma_tim2_ch1.Init.MemInc = DMA_MINC_ENABLE;

  hdma_tim2_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

  hdma_tim2_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

  hdma_tim2_ch1.Init.Mode = DMA_NORMAL;

  hdma_tim2_ch1.Init.Priority = DMA_PRIORITY_LOW;

  hdma_tim2_ch1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

   

   /* Several peripheral DMA handle pointers point to the same DMA handle.

   Be aware that there is only one channel to perform all the requested DMAs. */

  __HAL_LINKDMA(htim_ic, hdma[TIM_DMA_ID_CC1], hdma_tim2_ch1);

   

 }

  if (htim_ic->Instance == TIM5) {

  /* Peripheral clock enable */

  __TIM5_CLK_ENABLE();

  /* Peripheral DMA init*/

  hdma_tim5_ch4_trig.Instance = DMA1_Stream1;

  hdma_tim5_ch4_trig.Init.Channel = DMA_CHANNEL_6;

  hdma_tim5_ch4_trig.Init.Direction = DMA_PERIPH_TO_MEMORY;

  hdma_tim5_ch4_trig.Init.PeriphInc = DMA_PINC_DISABLE;

  hdma_tim5_ch4_trig.Init.MemInc = DMA_MINC_ENABLE;

  hdma_tim5_ch4_trig.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

  hdma_tim5_ch4_trig.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

  hdma_tim5_ch4_trig.Init.Mode = DMA_NORMAL;

  hdma_tim5_ch4_trig.Init.Priority = DMA_PRIORITY_LOW;

  hdma_tim5_ch4_trig.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

   

  

  HAL_DMA_Init(&hdma_tim5_ch4_trig);

   

   /* Several peripheral DMA handle pointers point to the same DMA handle.

   Be aware that there is only one channel to perform all the requested DMAs. */

  __HAL_LINKDMA(htim_ic, hdma[TIM_DMA_ID_CC1], hdma_tim5_ch4_trig);

 }

}

void MX_DMA_Init(void)

{

 /* DMA controller clock enable */

// __DMA1_CLK_ENABLE();

  __HAL_RCC_DMA1_CLK_ENABLE();

// /* DMA interrupt init */

// /* DMA1_Stream1_IRQn interrupt configuration */

  HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);

  HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);

  /* DMA1_Stream5_IRQn interrupt configuration */

  HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);

  HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0