Skip to main content
Dudenkov.Vladimir
Associate II
June 29, 2020
Question

I am can not update burst mode controller from any trigger.

  • June 29, 2020
  • 1 reply
  • 796 views

Im enable pwm output TA1, TA2 and try enable burst mode with changeble BMCMP and BMPER. Im change this registers and try update from timer triggers and software trigger, but pwm output set one burst state and doesnt change. Pwm burst state is updated if turn off and turn on BME bit.

stm32g474ret6

This topic has been closed for replies.

1 reply

Dudenkov.Vladimir
Associate II
June 29, 2020

This is example of my code

#define PWM_MIN_DUTY_CYCLE_VALUE 		700
static int16_t PWMvalueISR = PWM_MIN_DUTY_CYCLE_VALUE;
static int16_t PWMvalueDbg = PWM_MIN_DUTY_CYCLE_VALUE;
static uint32_t pulseIdle[] = 		{7, 3, 5, 1, 3, 1, 1};
static uint32_t pulsePeriod[] = 	{8, 4, 8, 2, 8, 4, 8};
static HRTIM_HandleTypeDef hhrtim1 = {0};
static void periph_hrtimPwmOutputInit(void)
{
	__HAL_RCC_GPIOA_CLK_ENABLE();
	__HAL_RCC_ADC12_CLK_ENABLE();
	__HAL_RCC_HRTIM1_CLK_ENABLE();
	
	GPIO_InitTypeDef gpio;
	
	//HRTIM CHA1 & CHA2
	gpio.Alternate = GPIO_AF13_HRTIM1;
	gpio.Mode = GPIO_MODE_AF_PP;
	gpio.Pull = GPIO_NOPULL;
	gpio.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	gpio.Pin = GPIO_PIN_8 | GPIO_PIN_9;
	HAL_GPIO_Init(GPIOA, &gpio);
	
	//ADC
	gpio.Alternate = 0;
	gpio.Mode = GPIO_MODE_ANALOG;
	gpio.Pull = GPIO_NOPULL;
	gpio.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	gpio.Pin = GPIO_PIN_0;
	HAL_GPIO_Init(GPIOA, &gpio);
	
	//ADC REGULATOR
	hadc1_regulator.Instance = ADC1;
	hadc1_regulator.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
	hadc1_regulator.Init.ContinuousConvMode = DISABLE;
	hadc1_regulator.Init.DataAlign = ADC_DATAALIGN_LEFT;
	hadc1_regulator.Init.DiscontinuousConvMode = DISABLE;
	hadc1_regulator.Init.DMAContinuousRequests = DISABLE;
	hadc1_regulator.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
	hadc1_regulator.Init.ExternalTrigConv = ADC_EXTERNALTRIG_HRTIM_TRG1;
	hadc1_regulator.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
	hadc1_regulator.Init.GainCompensation = 0;
	hadc1_regulator.Init.LowPowerAutoWait = DISABLE;
	hadc1_regulator.Init.NbrOfConversion = 1;
	hadc1_regulator.Init.NbrOfDiscConversion = 0;
	hadc1_regulator.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
	hadc1_regulator.Init.OversamplingMode = DISABLE;
	hadc1_regulator.Init.Resolution = ADC_RESOLUTION_12B;
	hadc1_regulator.Init.SamplingMode = ADC_SAMPLING_MODE_BULB;
	hadc1_regulator.Init.ScanConvMode = ADC_SCAN_DISABLE;
	HAL_ADC_Init(&hadc1_regulator);
	HAL_ADCEx_Calibration_Start(&hadc1_regulator, ADC_SINGLE_ENDED);
	
	ADC_MultiModeTypeDef multimode = {0};
	multimode.Mode = ADC_MODE_INDEPENDENT;
	HAL_ADCEx_MultiModeConfigChannel(&hadc1_regulator, &multimode);
	
	ADC_ChannelConfTypeDef adcChannelCfg = {0};
	adcChannelCfg.Channel = ADC_CHANNEL_1;
	adcChannelCfg.Offset = 2482; //target
	adcChannelCfg.OffsetNumber = ADC_OFFSET_1;
	adcChannelCfg.OffsetSaturation = DISABLE;
	adcChannelCfg.OffsetSign = ADC_OFFSET_SIGN_NEGATIVE;
	adcChannelCfg.Rank = ADC_REGULAR_RANK_1;
	adcChannelCfg.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
	adcChannelCfg.SingleDiff = ADC_SINGLE_ENDED;
	HAL_ADC_ConfigChannel(&hadc1_regulator, &adcChannelCfg);
	
	HAL_NVIC_SetPriority(ADC1_2_IRQn, 2, 0);
 HAL_NVIC_EnableIRQ(ADC1_2_IRQn);
	HAL_ADC_Start_IT(&hadc1_regulator);
	
	hhrtim1.Instance = HRTIM1;
	hhrtim1.Init.HRTIMInterruptResquests = HRTIM_IT_NONE;
	hhrtim1.Init.SyncInputSource = HRTIM_SYNCINPUTSOURCE_NONE;
	hhrtim1.Init.SyncOutputSource = HRTIM_SYNCOUTPUTSOURCE_MASTER_CMP1;
	hhrtim1.Init.SyncOutputPolarity = HRTIM_SYNCOUTPUTPOLARITY_POSITIVE;
	hhrtim1.Init.SyncOptions = HRTIM_SYNCOPTION_NONE;
	HAL_HRTIM_Init(&hhrtim1);
	HAL_HRTIM_DLLCalibrationStart(&hhrtim1, HRTIM_CALIBRATIONRATE_3);
	HAL_HRTIM_PollForDLLCalibration(&hhrtim1, 100);
	
	//hrtim
	HRTIM_TimeBaseCfgTypeDef timeBaseCfg = {0};
	timeBaseCfg.PrescalerRatio = HRTIM_PRESCALERRATIO_MUL32;
	timeBaseCfg.Period = 54400;
	timeBaseCfg.RepetitionCounter = 0;
	timeBaseCfg.Mode = HRTIM_MODE_CONTINUOUS;
	HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &timeBaseCfg);
	HAL_HRTIM_TimeBaseConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &timeBaseCfg);
	
	//hrtimv2 settings
	HRTIM_TimerCtlTypeDef timerCtl = {0};
	timerCtl.UpDownMode = HRTIM_TIMERUPDOWNMODE_UP;
	timerCtl.TrigHalf = HRTIM_TIMERTRIGHALF_DISABLED;
	timerCtl.GreaterCMP1 = HRTIM_TIMERGTCMP1_EQUAL;
	timerCtl.GreaterCMP3 = HRTIM_TIMERGTCMP3_EQUAL;
	timerCtl.DualChannelDacEnable = HRTIM_TIMER_DCDE_DISABLED;
	timerCtl.DualChannelDacStep = 0; //not used
	timerCtl.DualChannelDacReset = 0; //not used
	HAL_HRTIM_WaveformTimerControl(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &timerCtl);
	
	//timers common settings
	HRTIM_TimerCfgTypeDef timerCfg = {0};
	timerCfg.DMARequests = HRTIM_TIM_DMA_NONE;
	timerCfg.DMASrcAddress = 0x0;
	timerCfg.DMADstAddress = 0x0;
	timerCfg.DMASize = 0x1;
	timerCfg.HalfModeEnable = HRTIM_HALFMODE_DISABLED;
	timerCfg.StartOnSync = HRTIM_SYNCSTART_DISABLED;
	timerCfg.ResetOnSync = HRTIM_SYNCRESET_DISABLED;
	timerCfg.DACSynchro = HRTIM_DACSYNC_NONE;
 timerCfg.UpdateGating = HRTIM_UPDATEGATING_INDEPENDENT;
 timerCfg.BurstMode = HRTIM_TIMERBURSTMODE_MAINTAINCLOCK;
 timerCfg.PushPull = HRTIM_TIMPUSHPULLMODE_DISABLED;
 timerCfg.FaultLock = HRTIM_TIMFAULTLOCK_READWRITE;
 timerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE;
 timerCfg.DelayedProtectionMode = HRTIM_TIMER_A_B_C_DELAYEDPROTECTION_DISABLED;
 timerCfg.PreloadEnable = HRTIM_PRELOAD_ENABLED;
 timerCfg.DeadTimeInsertion = HRTIM_TIMDEADTIMEINSERTION_DISABLED;
 timerCfg.ResetUpdate = HRTIM_TIMUPDATEONRESET_DISABLED;
	timerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_ENABLED;
	timerCfg.BalancedIdleAutomaticResume = HRTIM_OUTPUTBIAR_DISABLED;
	timerCfg.InterleavedMode = HRTIM_INTERLEAVED_MODE_DISABLED;
	timerCfg.ReSyncUpdate = HRTIM_TIMERESYNC_UPDATE_UNCONDITIONAL;
	timerCfg.UpdateTrigger = HRTIM_TIMUPDATETRIGGER_MASTER;
	timerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_NONE;
	timerCfg.InterruptRequests = HRTIM_TIM_IT_NONE;
	HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, &timerCfg);
	
	//comparators settings
	HRTIM_CompareCfgTypeDef compareCfg = {0};
	compareCfg.AutoDelayedMode = HRTIM_AUTODELAYEDMODE_REGULAR;
	compareCfg.AutoDelayedTimeout = 0;
	
	compareCfg.CompareValue = 700;
	HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_1, &compareCfg);
	compareCfg.CompareValue = (700/2);
	HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_2, &compareCfg);
	compareCfg.CompareValue = (700/2) + 700;
	HAL_HRTIM_WaveformCompareConfig(&hhrtim1, HRTIM_TIMERINDEX_MASTER, HRTIM_COMPAREUNIT_3, &compareCfg);
	
	//output settings
	HRTIM_OutputCfgTypeDef outputCfg = {0};
	outputCfg.Polarity = HRTIM_OUTPUTPOLARITY_HIGH;
 outputCfg.IdleMode = HRTIM_OUTPUTIDLEMODE_IDLE;
 outputCfg.IdleLevel = HRTIM_OUTPUTIDLELEVEL_INACTIVE;
 outputCfg.FaultLevel = HRTIM_OUTPUTFAULTLEVEL_INACTIVE;
 outputCfg.ChopperModeEnable = HRTIM_OUTPUTCHOPPERMODE_DISABLED;
 outputCfg.BurstModeEntryDelayed = HRTIM_OUTPUTBURSTMODEENTRY_REGULAR;
	
	outputCfg.SetSource = HRTIM_OUTPUTSET_MASTERPER;
	outputCfg.ResetSource = HRTIM_OUTPUTRESET_MASTERCMP1;
	HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA1, &outputCfg);
	
	outputCfg.SetSource = HRTIM_OUTPUTSET_MASTERCMP2;
	outputCfg.ResetSource = HRTIM_OUTPUTRESET_MASTERCMP3;
	HAL_HRTIM_WaveformOutputConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, HRTIM_OUTPUT_TA2, &outputCfg);
	
	//burst controller
	HRTIM_BurstModeCfgTypeDef pBurstModeCfg = {0};
	pBurstModeCfg.Mode = HRTIM_BURSTMODE_CONTINOUS;
	pBurstModeCfg.ClockSource = HRTIM_BURSTMODECLOCKSOURCE_MASTER;
	pBurstModeCfg.Prescaler = HRTIM_BURSTMODEPRESCALER_DIV1;
	pBurstModeCfg.PreloadEnable = HRIM_BURSTMODEPRELOAD_ENABLED;
	pBurstModeCfg.Trigger = HRTIM_BURSTMODETRIGGER_MASTER_RESET;
	pBurstModeCfg.IdleDuration = pulseIdle[6];
	pBurstModeCfg.Period = pulsePeriod[6];
	HAL_HRTIM_BurstModeConfig(&hhrtim1, &pBurstModeCfg);
	
	//adc trigger
	HRTIM_ADCTriggerCfgTypeDef adcTriggerCfg = {0};
	adcTriggerCfg.Trigger = HRTIM_ADCTRIGGEREVENT24_MASTER_PERIOD | HRTIM_ADCTRIGGEREVENT24_MASTER_CMP2;
	adcTriggerCfg.UpdateSource = HRTIM_ADCTRIGGERUPDATE_MASTER;
	HAL_HRTIM_ADCTriggerConfig(&hhrtim1, HRTIM_ADCTRIGGER_1, &adcTriggerCfg);
	
	HAL_HRTIM_WaveformOutputStart(&hhrtim1, HRTIM_OUTPUT_TA1 | HRTIM_OUTPUT_TA2);
	HAL_HRTIM_WaveformCountStart(&hhrtim1, HRTIM_TIMERID_TIMER_A) != HAL_OK);
	HAL_HRTIM_WaveformCountStart(&hhrtim1, HRTIM_TIMERID_MASTER) != HAL_OK);
}
 
void ADC1_2_IRQHandler(void)
{
	__HAL_ADC_CLEAR_FLAG(&hadc1_regulator, ADC_FLAG_EOC);
	
	if(PWMvalueISR < PWMvalueDbg)
		++PWMvalueISR;
	else if(PWMvalueISR > PWMvalueDbg)
		--PWMvalueISR;
	break;
	
	//if < PWM_MIN_DUTY_CYCLE_VALUE ~ turn on burst mode
	if(PWMvalueISR < PWM_MIN_DUTY_CYCLE_VALUE)
	{
		hhrtim1.Instance->sCommonRegs.BMCMPR = pulseIdle[PWMvalueISR / 100];
		hhrtim1.Instance->sCommonRegs.BMPER = pulsePeriod[PWMvalueISR / 100];
		HAL_HRTIM_BurstModeCtl(&hhrtim1, HRTIM_BURSTMODECTL_ENABLED);
		HAL_HRTIM_BurstModeSoftwareTrigger(&hhrtim1);
		
		__HAL_HRTIM_SETCOMPARE(&hhrtim1,HRTIM_TIMERINDEX_MASTER,HRTIM_COMPAREUNIT_1,PWM_MIN_DUTY_CYCLE_VALUE);
		__HAL_HRTIM_SETCOMPARE(&hhrtim1,HRTIM_TIMERINDEX_MASTER,HRTIM_COMPAREUNIT_3,27200+PWM_MIN_DUTY_CYCLE_VALUE);
	}//if > PWM_MIN_DUTY_CYCLE_VALUE ~ turn off burst mode
	else
	{
		HAL_HRTIM_BurstModeCtl(&hhrtim1, HRTIM_BURSTMODECTL_DISABLED);
		HAL_HRTIM_BurstModeSoftwareTrigger(&hhrtim1);
		
		__HAL_HRTIM_SETCOMPARE(&hhrtim1,HRTIM_TIMERINDEX_MASTER,HRTIM_COMPAREUNIT_1,PWMvalueISR);
		__HAL_HRTIM_SETCOMPARE(&hhrtim1,HRTIM_TIMERINDEX_MASTER,HRTIM_COMPAREUNIT_3,27200+PWMvalueISR);
	}
}