Skip to main content
serefatakan
Associate
February 11, 2019
Solved

HW timers with FreeRTOS

  • February 11, 2019
  • 4 replies
  • 4249 views

Hi,

I am struggling with HW timers when using FreeRTOS. Using H743ZI Nucleo Board and writing on FreeRTOS application examples.

I have changed ThreadCreation application a little bit: created another task that initializes LEDs and a timer, and creates other 2 tasks.

In the modified application, I have tried to setup a timer to get interrupts in every 4 us that only blinks an LED. None of LEDs were blinking and when debugging paused, system goes Default_Handler.

If I comment out timer part, FreeRTOS and tasks works fine; if osKernelStart() line is commented out, timer and interrupt works fine. But I need both so any help will be magnificent.

Here is some part of code:

int main(void)
{
 /* Enable the CPU Cache */
 CPU_CACHE_Enable();
 
 
 HAL_Init();
 
 /* Configure the system clock to 400 MHz */
 SystemClock_Config();
 
 /* Init thread definition */
 osThreadDef(INIT, Init_Thread, osPriorityNormal, 0, configMINIMAL_STACK_SIZE);
 
 /* Start thread 1 */
 InitThreadHandle = osThreadCreate(osThread(INIT), NULL);
 
 /* Start scheduler */
 osKernelStart();
 
 /* We should never get here as control is now taken by the scheduler */
 for (;;);
 
}

And initialization thread (Other threads are same as example):

static void Init_Thread(void const *argument)
{
	TIM_HandleTypeDef TimHandle;
	uint8_t asdf;
 
	/* Initialize LEDs */
	BSP_LED_Init(LED1);
	BSP_LED_Init(LED2);
 
	__HAL_RCC_TIM3_CLK_ENABLE();
 
	TimHandle.Instance = TIM3;
 
	TimHandle.Init.Period = 560;
	TimHandle.Init.Prescaler = 1;
	TimHandle.Init.ClockDivision = 0;
	TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
	TimHandle.Init.RepetitionCounter = 0;
	TimHandle.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 
	/* TIM13 interrupt Init */
	HAL_NVIC_SetPriority(TIM3_IRQn, 0, 0);
	HAL_NVIC_EnableIRQ(TIM3_IRQn);
 
	asdf = HAL_TIM_Base_Init(&TimHandle);
	configASSERT(!asdf);
 
	/*##-2- Start the TIM Base generation in interrupt mode ####################*/
	/* Start Channel1 */
	asdf = HAL_TIM_Base_Start_IT(&TimHandle);
	configASSERT(!asdf);
 
	/* Thread 1 definition */
	osThreadDef(LED1, LED_Thread1, osPriorityNormal, 0, configMINIMAL_STACK_SIZE);
 
	/* Thread 2 definition */
	osThreadDef(LED2, LED_Thread2, osPriorityNormal, 0, configMINIMAL_STACK_SIZE);
 
	/* Start thread 1 */
	LEDThread1Handle = osThreadCreate(osThread(LED1), NULL);
 
	/* Start thread 2 */
	LEDThread2Handle = osThreadCreate(osThread(LED2), NULL);
 
	for(;;) osThreadTerminate(NULL);
}

And the IRQHandler:

static void TIM3_IRQHandler(void)
{
	BSP_LED_Toggle(LED3);
}

This topic has been closed for replies.
Best answer by Chris1

Minimally, since you have enabled the TIM Update event:

static void TIM3_IRQHandler(void)
{
 __HAL_TIM_CLEAR_IT(&TimHandle, TIM_IT_UPDATE); 
 // clear TIM interrupt pending bit
  BSP_LED_Toggle(LED3);
}

4 replies

Tesla DeLorean
Guru
February 11, 2019

Unless your IRQ Handler clears the source it is going to be re-entering indefinitely.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
serefatakan
Associate
February 12, 2019

Hi Clive, thank you for reply.

What do you mean by clearing sources? Is the problem about timer initialization? Can you show me an example?

Chris1
Chris1Best answer
Associate II
February 12, 2019

Minimally, since you have enabled the TIM Update event:

static void TIM3_IRQHandler(void)
{
 __HAL_TIM_CLEAR_IT(&TimHandle, TIM_IT_UPDATE); 
 // clear TIM interrupt pending bit
  BSP_LED_Toggle(LED3);
}

serefatakan
Associate
February 13, 2019

Thank you both, my inattention.