cancel
Showing results for 
Search instead for 
Did you mean: 

How use X-CUBE-DSPDEMO with a STM32H7xx card (and not F7...) ?

erinndalria
Associate

Hi everybody !

I've tried to implement the additional features given in X-CUBE-DSPDEMO (to use, for exemple FFT) to a project for my STM32H743I_EVAL board. The "H7" has like "F7" the ARM M7 in it so it says that DSP operation could be implemented on F4, H4, F7 and H7 cards.

However the additionnal package for the Cube is only available for F series. I tried to change many files but I doesn't work and I'm not sure that is the bes idea to do.

I'm almost a newbie on STM32 trying to understand this new "tool".

Has anyone tried to use DPS features, FFT, etc. on this kind of board ?

Thanks for your help :) (if there is already a topic about that, sorry for the repost...)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0