Skip to main content
HJun
Visitor II
Jun 27, 2019 2:46 AM UTC
Question

How to use at the same time [TIM1 Encoder interface mode and PWM generation mode]

Hi, I use STM32F103VBT.

Can anyone provide an example of how to use TIM1 Encoder interface mode(ch1, ch2) and PWM generation mode(ch3, ch4) at the same time?

​

PWM ​operation is stopped when encoder interface mode on.

TIM_EncoderInterfaceConfig(TIM1,TIM_EncoderMode_TI12,TIM_ICPolarity_Rising, TIM_ICPolarity_Rising);

my source code is below:

void TIMER1_Initialize(void)

{

 TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

 TIM_OCInitTypeDef TIM_OCInitStructure;  

 TIM_ICInitTypeDef TIM_ICInitStructure;

  

 TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);

 // TIM1 clock enable 

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);  

 /* Time base configuration */     

 TIM_TimeBaseStructure.TIM_Period = 200-1; // MAX 0xFFFF   

 TIM_TimeBaseStructure.TIM_Prescaler = 10-1;  //1khz

 TIM_TimeBaseStructure.TIM_ClockDivision = 0;

 TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

 //TIM_EncoderInterfaceConfig(TIM1,TIM_EncoderMode_TI12,TIM_ICPolarity_Rising, TIM_ICPolarity_Rising);

  

 TIM_ICInitStructure.TIM_Channel=TIM_Channel_1;

 TIM_ICInitStructure.TIM_ICFilter=0; 

 TIM_ICInit(TIM1, &TIM_ICInitStructure);

 TIM_ICInitStructure.TIM_Channel=TIM_Channel_2;

 TIM_ICInitStructure.TIM_ICFilter=0;

 TIM_ICInit(TIM1, &TIM_ICInitStructure);

 TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

 TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

 // PWM1 Mode configuration: Channel3 

 TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

 TIM_OCInitStructure.TIM_Pulse = 20;

 TIM_OC3Init(TIM1, &TIM_OCInitStructure);

 TIM_OC3PreloadConfig(TIM1, TIM_OCPreload_Enable);

 // PWM1 Mode configuration: Channel4 

 TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

 TIM_OCInitStructure.TIM_Pulse = 1;

 TIM_OC4Init(TIM1, &TIM_OCInitStructure);

 TIM_OC4PreloadConfig(TIM1, TIM_OCPreload_Enable);

  

 TIM_CtrlPWMOutputs(TIM1, ENABLE);

 TIM_ARRPreloadConfig(TIM1, ENABLE);

 // TIM1 enable counter 

 TIM_Cmd(TIM1, ENABLE);

 // Enable the CC Interrupt Request 

 TIM_ClearFlag(TIM1, TIM_FLAG_Update);

 TIM_ITConfig(TIM1, TIM_IT_CC1, ENABLE);

}

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Jun 27, 2019 6:35 AM UTC

> Can anyone provide an example of how to use TIM1 Encoder interface mode(ch1, ch2) and PWM generation mode(ch3, ch4) at the same time?

You can't.

There is only one counter in the timer. It either counts the encoder pulses, or it runs out of the APB clock, can't do both at the same time.

JW