2025-01-10 08:03 PM
Hi everyone,
I am currently working on a project involving the ST25DV NFC tag connected to a microcontroller (STM32). My goal is to test the Fast Transfer Mode (FTM) functionality. Here's the workflow I am aiming to achieve:
1. An NFC device (e.g., a smartphone) sends an FTM response/request to the ST25DV tag.
2. The microcontroller receives the FTM request/response from the ST25DV NFC tag and handles it accordingly.
I am looking for guidance on the following:
How can I simulate and verify the full FTM communication flow (NFC device ↔ ST25DV ↔ MCU)?
Are there any specific tools or software recommendations for testing FTM functionality?
Can I use ST25 NFC app to test FTM? Understand there is a app to test FTM demo using ST25 discovery kits. However I just need to test the transaction like send request to MCU thought FTM.
Regards,
2025-01-10 09:15 PM
Testing FTM functionality with an ST25DV tag and an MCU can be achieved through a combination of hardware and software tools. Here's a breakdown of the process and recommendations: