2021-10-05 8:32 AM
Hi,
I am using STM32F746G_DISCOVERY board.
In the QSPI_PreInitConfig example, how to put const array data to QSPI flash? I try to declare as follows, but cannot pass compiler. error: 'img2' causes a section type conflict with 'GpioToggle'. I notice that section(".qspi") is used by function GpioToggle(), I should make array data share the same section in QSPI memory, not sure how to do it. The following is the code with compiler error.
__attribute__((section(".qspi")))
const unsigned char img2[2] =
{
0xFF, 0xFF
};
2021-10-05 10:13 AM
/* Memory Spaces Definitions */
MEMORY
{
...
QSPI (rx) : ORIGIN = 0x90000000, LENGTH = 1M
}
...
.qspi :
{
*(.qspi)
*(.qspi.*)
} >QSPIIn .C
__attribute__((section(".qspi")))
const unsigned char img2[2] =
{ 0xFF, 0xFF };
...
In .MAP
.qspi 0x90000000 0x2
*(.qspi)
.qspi 0x90000000 0x2 out/main.o
0x90000000 img2
*(.qspi.*)Would take time/effort to set up a build system for the project you mention, I did this with existing GNU build environment I use.
Figure out why your compiler is annoyed, and associating this with GpioToggle(), et al
2021-10-05 5:54 PM
I created .qspi2 section in the linker file:
.qspi :
{
. = ALIGN(4);
_qspi_start = .; /* create a global symbol at qspi start */
*(.qspi) /* .qspi sections */
*(.qspi*) /* .qspi* sections */
*(.qspi2) /* .qspi2 sections */
*(.qspi2*) /* .qspi2* sections */
. = ALIGN(4);
_qspi_end = .; /* define a global symbols at end of qspi */
} >QSPI
===========
and declare img2 as:
__attribute__((section(".qspi2")))
const uint16_t img2[2] =
{
0xFF, 0xFF
};
===========
GpioToggle is still the same:
static void __attribute__((section(".qspi"), noinline)) GpioToggle(void)
now compiler error goes away.
But the .list file does not show any memory allocated for img2[].
Still not sure how to allocate memory for img2[] in QSPI memory space starting at 0x90000000.
I can send project folder if you like.
Please help.
2021-10-05 9:31 PM
Perhaps if the text and data name spaces conflict
__attribute__((section(".qspi.data"))) // this will match against *(.qspi.*)
const uint16_t img2[2] =
{
0xFF, 0xFF
};
2021-10-06 7:50 AM
I changed to __attribute__((section(".qspi.data"))), but still don’t see img2 memory allocation.
Now I only use img2[] for .qspi section, GpioToggle function is moved outside .qspi section.
The beginning of list file shows as follows, .qspi has size of 0. Img2[] is not allocated in .qspi.
==================
Sections:
Idx Name Size VMA LMA File off Algn
0 .isr_vector 000001c8 08000000 08000000 00010000 2**0
CONTENTS, ALLOC, LOAD, READONLY, DATA
1 .text 00000f94 080001c8 080001c8 000101c8 2**2
CONTENTS, ALLOC, LOAD, READONLY, CODE
2 .rodata 00000018 0800115c 0800115c 0001115c 2**2
CONTENTS, ALLOC, LOAD, READONLY, DATA
3 .qspi 00000000 90000000 90000000 0002000c 2**0
CONTENTS
4 .init_array 00000004 08001174 08001174 00011174 2**2
CONTENTS, ALLOC, LOAD, DATA
2021-10-06 8:14 AM
Linker can discard unused data objects. Use it somewhere.
2021-10-06 2:21 PM
Linker Script can be forced to "keep" sections, entry points, etc
/* Ensure entry points are pulled in here */
KEEP (*(.text.Init))
KEEP (*(.text.Write))
KEEP (*(.init))
KEEP (*(.fini))
There's also the used attribute, although I found that to be less than effect.
__attribute__((used))
2021-10-06 6:19 PM
Thanks for the help!
I figured out. I should put array in .h file, not c file.