2026-01-12 3:43 AM - last edited on 2026-01-12 4:35 AM by Andrew Neil
Environment:
STM32F407VGTX
USB HID mouse, Full Speed
Problem:
Hi, I’m using a STM32F407VGTX board. I send a USB remote wakeup signal to the host and then try to receive a resume signal from the host. The STM32 board can wake up the host (bringing it to the login screen), but it cannot trigger the USB_OTG_GINTSTS_WKUINT interrupt. I have already configured my STM32 board as a HID mouse. However, if I use a real mouse instead, it can wake up the host and successfully trigger the USB_OTG_GINTSTS_WKUINT interrupt. Is there any suggestion or workaround for this problem?
void usb_remote_wakeup()
{
if (hUsbDeviceFS.dev_remote_wakeup == 1)
{
__HAL_PCD_UNGATE_PHYCLOCK(&hpcd_USB_OTG_FS);
HAL_PCD_ActivateRemoteWakeup(&hpcd_USB_OTG_FS);
HAL_Delay(5);
HAL_PCD_DeActivateRemoteWakeup(&hpcd_USB_OTG_FS);
}
}
2026-01-12 6:37 AM
Hello @Harry0709
You can refer to the USB HID application available in the STM32CubeF4 firmware:
HID application support remote wakeup
If you are not able to trigger the USB_OTG_GINTSTS_WKUINT interrupt, you can share with me how you are trying to trigger it, and I will help you
best regards,
hamdi