cancel
Showing results for 
Search instead for 
Did you mean: 

compatibility between LL library of stm32f4 and stm32f7

elmzaiti youssef
Associate II
Posted on July 12, 2017 at 13:35

the LL library of the stm32f4xx and stm32f7xx , is the same ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on July 12, 2017 at 14:14

Hello

youssef.elmzaiti

,

To see more about Low layer drivers on STM32F7 and STM32F4, refer to the user manual:

With Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Tilen MAJERLE
ST Employee
Posted on July 14, 2017 at 10:24

Hello

youssef.elmzaiti

‌,

LL libraries are designed for very low-level tasks and there is general compatibility between them, but this is not the case for all peripherals. There can be incompatibility and some functions which exists in F7, are not available on F4, depends on device features, and vice-versa of course.

Posted on July 19, 2017 at 15:49

 ,

 ,

2017-07-14 10:24 GMT+02:00 Tilen MAJERLE <,st-microelectronics@jiveon.com>,:

STMicroelectronics Community

<,https://community.st.com/?et=notification.mention>,

You have been mentioned

by Tilen MAJERLE

<,

Re: compatibility between LL library of stm32f4 and stm32f7 in

STMicroelectronics Community* - View Tilen MAJERLE's reference to you

<,https://community.st.com/0D70X000006Sp8aSAC