How to place a variable into the CCM SRAM using the scatter file?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-20 7:09 AM
I'm using the arm_rfft_fast_f32 function, I write a scatter file and place some library files in the CCM SRAM like below, and the speed is faster.
RW_IRAM2 0x10000000 0x00002800 { ; CCM SRAM 10kB
.ANY (ccmram)
arm_rfft_fast_f32.o (+RO)
arm_cfft_f32.o (+RO)
arm_cfft_radix8_f32.o (+RO)
arm_rfft_fast_init_f32.o (+RO)
}
but the twiddleCoef tables in arm_common_tables.o are too large to fit into the CCM SRAM, how to place the table "twiddleCoef_256" into the CCM SRAM specifically? Other tables are useless in my app.
Thanks!
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0