2020-11-29 12:19 PM
My stm32 mcu is a i2c slave device.
Generally, I2C slaves have a dedicated register for a specific data. But since this is stm32 mcu it does not have a resister map to store different kind of data in a separate register. It has to interpret everything from what it receives in the RXDR register.
2020-11-29 7:02 PM
Which STM32? There are hundreds of chips.
Generally, you will want to interpret the incoming bytes as you receive them. The I2C peripheral is complicated, you need to interpret in realtime and populate outgoing buffers accordingly.
If you're a fan of HAL, look at some examples:
2020-11-29 8:51 PM
@TDK This is STM32G031. Is there a way to define a protocol between master and slave so that slave can do some interpretation?
I am currently using the Slave Receive HAL API to receive data into a buffer,
uint8_t data[10];
HAL_I2C_Slave_Receive_IT(&hi2c1, data, sizeof(data))
2020-11-30 5:17 AM
> Is there a way to define a protocol between master and slave so that slave can do some interpretation?
Of course. The only limitation to this is your ability to program that protocol. I2C is complicated, particularly if you're using interrupts. It may take some time to figure out. I would start with blocking calls and progress to non-blocking once that is working.
2020-12-02 7:13 PM
@TDK Thanks ! Any ideas on point 1 in my orginal question
My stm32 mcu is a i2c slave device.
I am using Listen Mode APIs as below,
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c,
uint8_t TransferDirection,
uint16_t AddrMatchCode)
{
if(hi2c->Instance == I2C1)
{
uint8_t id = 0xA0;
if(TransferDirection == I2C_DIRECTION_TRANSMIT)
HAL_I2C_Slave_Seq_Receive_IT(&hi2c1, data, sizeof(data),I2C_FIRST_FRAME);
else
HAL_I2C_Slave_Seq_Transmit_IT(&hi2c1, &id, 1, I2C_LAST_FRAME);
}
}
int main(void)
{
....
while(1)
{
....
HAL_I2C_EnableListen_IT(&hi2c1);
}
}Every-time I send a read command, it enter HAL_I2C_Slave_Transmit_IT but does not send out the data. Because inside the IRQ handler there is condition which checks the ADDR flag and since that is true it just returns from there.
2020-12-02 7:22 PM