2017-09-18 3:33 AM
While generating STM32H743 project by CubeMX, I noticed that FDCAN1 can be either 'master mode' or 'full-duplex mode', and they map to different pairs of signal pins ( FDCAN1_TX/RX and
FDCAN1_
TXFD/RXFD ).I found that
FDCAN1_
TX/RX works in both modes, butFDCAN1_TXFD/RXFD did not work in any mode.
The problem is that I have a need to make FDCAN1_TXFD/
FDCAN1_RXFD work, would anyone give me any advice? Thanks in advance!
2017-09-18 8:27 AM
Hi
aaron_chang
,can you share with us which version of
http://www.st.com/en/development-tools/stm32cubemx.html
and which version ofhttp://www.st.com/en/embedded-software/stm32cubeh7.html
firmware you areusing ? If it is not already the case, can you try with STM32CubeMX v4.1 and STM32CubeH7 v1.1.0 ?Best regards,
Cedric
2017-09-18 8:30 PM
I was already using STM32CubeMX 4.22.1 and STM32Cube FW_H7 V1.1.0.
The CubeMX suggested me using PH15 and PI0 but did not generate any setting for those GPIOs.
So I added some code and set those GPIOs as ''Alternative Function 9 (FDCAN1)'', but they did not work.
Besides, I was wandering why those settings are ''n/a'', does that means the hardware is not ready for using yet?
Thank you for the response, and please let me know if you have any further thought.