2023-05-02 7:35 AM
I have a custom board with the l452cc controller. I am trying to run an sd card with fatfs through spi. I have generated cubemx fatfs files, but there is no interface layer for spi to fatfs. Are there some examples I can reference off of, or what is the best way to approach this?
Thanks.
Solved! Go to Solution.
2023-05-08 11:04 AM
Thanks for the input, I'll see how far I get and ask back if I have questions. Thanks
2023-05-08 6:36 PM
Is FatFS able to handle if SD card's sector size is not 512?
2023-05-08 6:37 PM
If you make it work, please also post your tech details here.
2023-05-09 6:12 AM
Well I'm making some progress. I implimented the NUCLEO-L452RE example project basically. 'BSP_SD_INIT()' returns success. f_mount however returns 'FR_NO_FILESYSTEM'. Sd card is a 16GB formatted with exFat currently. I have tried formatting it with FAT32 as well, with no success. Is this a low level problem, or is there something fundamentally wrong with my implimentation. Here is the section of applicable code.
static void SDCard_Config(void) {
/* Initialize the SD */
if (BSP_SD_Init() != MSD_OK) {
#if DEBUG
debug_printf("BSP_SD_INIT_FAILED\r\n");
#endif
} else {
#if DEBUG
debug_printf("BSP_SD_INIT_SUCCESS\r\n");
#endif
}
}void MX_FATFS_Init(void)
{
/*## FatFS: Link the USER driver ###########################*/
retUSER = FATFS_LinkDriver(&SD_Driver, USERPath);
/* USER CODE BEGIN Init */
/* additional user code for init */
/* USER CODE END Init */
}MX_FATFS_Init();
SDCard_Config();
FIL fil; /* File object */
char line[100]; /* Line buffer */
FRESULT fr; /* FatFs return code */
/* Give a work area to the default drive */
fr = f_mount(&SD_FatFs, "", 1);
if (fr) {
__NOP();
}
/* Open a text file */
fr = f_open(&fil, "message.txt", FA_READ);
if (fr) {
__NOP();
}
/* Read every line and display it */
while (f_gets(line, sizeof line, &fil)) {
debug_printf(line);
}
/* Close the file */
f_close(&fil);Thanks
2023-05-09 6:25 AM
2023-05-09 1:32 PM
So apparently 'Check boot record signature' is what is firing the error.
if (ld_word(fs->win + BS_55AA) != 0xAA55) return 3; /* Check boot record signature (always placed here even if the sector size is >512) */It would almost seem like I have a spi driver problem, but if I look in 'fs->win' there appears to be some random data lines 440 to 461 in the sector. So not sure if it is a driver problem or not.
2023-05-09 3:30 PM
Ok so it was a driver problem. I haven't pinned it down yet, but it has to do with the dma, because when I use normal spi mode, it will do a basic read write. So the process to get an sd card working is this:
Generate fatfs files with cubemx
Copy BSP package in from the adafruit sd shield example
Write a spi driver, and tie it into the BSP package
In theory it should then work. I may have missed a few details, so feel free to ask if you have any questions.
2023-05-09 6:30 PM
Are you able to read/write file with large size, like a few tens or even hundreds bytes?
How do you format the SD card? What is the sector size?
2023-05-10 5:47 AM
I haven't tried much besides a basic hello world text file. I will see here at some point. The card is formatted with FAT, and I have tried exFat too and that works. I will post back after I have tried some bigger files.
2023-05-10 6:42 AM
Well I don't know if this gets what you are wanting to know but here is a piece of code that I ran.
BYTE buf[2048];
memset(buf, 0x4c, sizeof(buf));
UINT br, bw;
fr = f_write(&fil, buf, sizeof(buf), &bw);The file when I look at it is filled with 0x4c, so it seems like it is working.