cancel
Showing results for 
Search instead for 
Did you mean: 

How to install the SD card Driver

rimbamor
Associate II
Posted on March 28, 2011 at 11:12

How to install the SD card Driver

3 REPLIES 3
Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:29

What did you try?

How did it fail?

Be specific.

rimbamor
Associate II
Posted on May 17, 2011 at 14:29

ok i m using STM3210C eval bord and i want to read a file from SD card , so first i should install the driver of the SDcard (it's connceted with SPI3)

I found an example stm32_eval_spi_sd.c  in

 

STM32 Embedded GUI library (AN3128)

\FIRMWARE\Utilities\STM32_EVAL\Common  

 I'can't understand how to configure pins of SDcard.

Andrew Neil
Evangelist III
Posted on May 17, 2011 at 14:29

Driving an SD-Card is not a trivial exercise.

Configuring the SPI interface is quite basic.

Is seems that you need to spend some time gaining familiarity with the basics of the STM32 and the STM3210C eval board before moving on to more advanced projects.

There are plenty of basic examples - including SPI - included with the standard peripheral library (aka ''FW Library'')

http://www.st.com/stonline/stappl/resourceSelector/app?page=resourceSelector&doctype=FIRMWARE&ClassID=1734