How to get the best ADC data?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-07-06 12:56 PM
I am testing/playing with a STM32f207 dev. board. I would like to know what ways are there to get most out of the ADC converter. For instance, is it possible to shut down the rest of CPU when conversion is done. Is there something ARM or ST specific I should know or are there any mistakes I made. The code below is mostly from the CubeMX.
The PC board is of course important and a dev. kit is not optimized for analog signals. Output wanders now between 0 and 3 and there are random high glitches. But some of it comes surely from the PCB. The program below calculates an average of two conversions.#include ''stm32f2xx_hal.h''
#include <string.h>
#include <stdio.h>
#include <stdlib.h>
/* USER CODE BEGIN Includes */
char
plaa[] =
''Hellogffgffgf''
;
char
klaa[20];
/* USER CODE END Includes */
float
kkk,ccc;
int
b,c;
/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
UART_HandleTypeDef huart3;
void
SystemClock_Config(
void
);
static
void
MX_GPIO_Init(
void
);
static
void
MX_ADC1_Init(
void
);
static
void
MX_USART3_UART_Init(
void
);
int
main(
void
)
{
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_USART3_UART_Init();
while
(1)
{
/* USER CODE END WHILE */
HAL_ADC_Start(& hadc1);
while
(HAL_OK!= HAL_ADC_PollForConversion(&hadc1, 1000))
{
}
ccc= HAL_ADC_GetValue(&hadc1);
HAL_ADC_Start(& hadc1);
while
(HAL_OK!= HAL_ADC_PollForConversion(&hadc1, 1000))
{
}
ccc= HAL_ADC_GetValue(&hadc1)+ccc;
kkk=ccc/2;
sprintf
(klaa,
''readout %f \n''
, kkk);
c=
sizeof
(klaa);
// strcpy(klaa,b);
HAL_UART_Transmit(&huart3,(uint8_t *) klaa,c,1000);
/* USER CODE BEGIN 3 */
HAL_UART_Receive(&huart3, (uint8_t *)klaa,
sizeof
(klaa), 1000);
HAL_UART_Transmit(&huart3,(uint8_t *) klaa,c,1000);
HAL_Delay(1000);
}
}
Clip
Clip
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-07-06 1:17 PM
There is a dedicated application note how to reduce noise on F20x/F405. With newer families, e.g.F42x and F401/F411, these problems are fixed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-07-06 2:36 PM
Thank you for your answer. I found two App notes that looked interesting.