ADC3_IN2 on STM32F427
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-06-30 4:16 PM
Existing code, ADC2_IN1 on PA1 works polled 100 numbers vary from 150 to 3050 sinusoid. HW guy added ADC3_IN2 on PA2.
Changed the code as below, but 100 numbers are all between 3013 and 3015, although can see a clipped sinusoid on Bitscope. Any ideas what to check? void ecg_init (void) { static GPIO_InitTypeDef GPIO_InitStructure; static ADC_InitTypeDef ADC_InitStructure; // [dy] ECG_OUT2 is on PA2 ADC3_IN2 RCC_AHB1PeriphClockCmd(BSP_ECG_ANALOG_INPUT_GPIO_RCC_AHB1_PERIPH, ENABLE); // [dy-ECG1] RCC_APB2PeriphClockCmd(BSP_ECG_ANALOG_INPUT_ADC_RCC_APB2_PERIPH, ENABLE); //[dy] RCC Enable for ECG2 RCC_APB2PeriphClockCmd(BSP_ECG2_ANALOG_INPUT_ADC_RCC_APB2_PERIPH, ENABLE); /* Configure GPIO (ECG) as analog input ******************************/ //[dy] GPIO_Pin_2 for ECG2 GPIO_InitStructure.GPIO_Pin = /* [dy-ECG1] BSP_ECG_ANALOG_INPUT_GPIO_PIN |*/ BSP_ECG2_ANALOG_INPUT_GPIO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(BSP_ECG_ANALOG_INPUT_GPIO_PORT, &GPIO_InitStructure); ssm_adc_common_init (); /* ADC ECG Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; // THIS WAS Different ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; // [dy-ECG1] ADC_Init(BSP_ECG_ANALOG_INPUT_ADC_NUM, &ADC_InitStructure); // [dy] ADC_Init for ECG2 ADC_Init(BSP_ECG2_ANALOG_INPUT_ADC_NUM, &ADC_InitStructure); // [dy] BSP_ECG2_ANALOG_INPUT_ADC_NUM ADC3 // NV 20130926 KEY Do this only once... #ifdef ECG1 ADC_RegularChannelConfig(BSP_ECG_ANALOG_INPUT_ADC_NUM, BSP_ECG_ANALOG_INPUT_ADC_CHANNEL, 1, ADC_SampleTime_3Cycles); ADC_Cmd(BSP_ECG_ANALOG_INPUT_ADC_NUM, ENABLE); #endif // [dy] BSP_ECG2_ANALOG_INPUT_ADC_CHANNEL ADC_Channel_2 ... ADC_RegularChannelConfig(BSP_ECG2_ANALOG_INPUT_ADC_NUM, BSP_ECG2_ANALOG_INPUT_ADC_CHANNEL, 1, ADC_SampleTime_3Cycles); ADC_Cmd(BSP_ECG2_ANALOG_INPUT_ADC_NUM, ENABLE); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-06-30 7:09 PM
Without the defines it's just a jumbled mess. Suggest you spend 5 minutes and code a clean free standing example from scratch where you explicitly code the pins, channel and adc, and test that. If that duplicates the behaviour you are seeing start digging at the hardware, if it works properly look at your defines.
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
‎2015-07-06 3:35 PM
Wrote a separate ecg2_init and changed to use ADC2 ADC_Channel_2 now works fine.