2026-06-01 8:48 PM
In my test environment, STM32H7S3Z8T6 works as the I3C controller and talks to the STM32H5 (I2C slave). The goal is STM32H7 will send out the entire SETDASA bytes at Legacy I2C speed, once STM32H5 receives the I2C speed SETDASA bytes, it decodes the sequence using software, and then switch from I2C slave to I3C target.
On I3C controller side (STM32H7), when I use the HAL availble CCC API below:
Once 0x7E broadcast addr ACKed by I2C slave, CCC (0x87) and the following address infomation will be sent only at I3C speed (which are controled by the hardware).
So, I switched to the following strategy using I2C private transfer under I3C mode:
But again, it turns out only 0x7E the broadcast address could be received by I2C slave.
In order to make sure STM32H7 can support legacy I2C speed in I3C mode, what is the necessary configration during bus initialization?
Will the above configurations work?
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.