How to config SYS_WKUP3 for STM32L4 MCU Standby mode?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-30 11:09 AM
Hi,
I am setting up STM32L4 for standby mode. From Cube and NUCLEO-L496ZG\Examples\PWR\PWR_SLEEP\Src the GPIO pin is PE6.
However I don't see any Cube generated code to init this pin. Neither in example code.
Should I init the PE6 as GPIO input pin?
Thx
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-30 11:56 AM
The example uses PC.13 (the user button)
Defined in
STM32Cube_FW_L4_V1.12.0\Drivers\BSP\STM32L4xx_Nucleo_144\stm32l4xx_nucleo_144.h
Initialized in
STM32Cube_FW_L4_V1.12.0\Drivers\BSP\STM32L4xx_Nucleo_144\stm32l4xx_nucleo_144.c
Also note the button makes to VDD, and the pin configured as Input, pull-down
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
‎2018-07-30 2:09 PM
Hi Clive,
I have following code modify for PE6 running Nucleo-144. However I am unable to breakpoint into EXTI15_10_IRQHandler() function.
Looking the code below, it setup the PE6 and EXTI15_10_IRQHandler but there is no connection between those two.
How can I setup the GPIO PE6 to EXTI15_10_IRQHandler?
Thx
else if (ButtonMode == BUTTON_MODE_EXTI)
{
/* Configure Button pin as input with External interrupt */
GPIO_InitStruct.Pin = BUTTON_PIN[Button];
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct);
/* Enable and set Button EXTI Interrupt to the lowest priority */
HAL_NVIC_SetPriority((IRQn_Type)(BUTTON_IRQn[Button]), 0x0F, 0x00);
HAL_NVIC_EnableIRQ((IRQn_Type)(BUTTON_IRQn[Button]));
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-30 3:23 PM
You'd use EXTI9_5_IRQHandler
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
‎2018-07-30 4:46 PM
Don't see this EXTI9_T_IRQHandler working.
Also strange for PE6, it's value always 1 even I connect to GND.
Thx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-30 5:18 PM
Evidently not doing something right.
Check schematic and connectivity. Check clocks
Use debugger, inspect all related registers.
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
‎2018-07-31 9:43 AM
I missed the clock enable code. for GPIOE.
__HAL_RCC_GPIOE_CLK_ENABLE();
But now I get 0 all the time for PE6.
Checking the user's manual, seems PE6 in CN9 is assigned to SAI_1_A. Not sure if I can use for SYS_WKUP3 although I am not using SAI.
If not how can we test SYS_WKUP3 on Nucleo-144 board?
Thx
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-07-31 10:18 AM
PE6 should be usable for this purpose.
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
‎2018-07-31 2:35 PM
Why there is a need to init GPIO pin different way for MODE_GPIO and MODE_EXTI?
What I need for this SYS_WKUP3 is whenever the GPIO value change interrup service routine will be called. In this case should I only have EXTI mode?
Thx
void BSP_PB_Init(Button_TypeDef Button, ButtonMode_TypeDef ButtonMode)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Enable the BUTTON Clock */
BUTTONx_GPIO_CLK_ENABLE(Button);
if (ButtonMode == BUTTON_MODE_GPIO)
{
/* Configure Button pin as input */
GPIO_InitStruct.Pin = BUTTON_PIN[Button];
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct);
}
else if (ButtonMode == BUTTON_MODE_EXTI)
{
/* Configure Button pin as input with External interrupt */
GPIO_InitStruct.Pin = BUTTON_PIN[Button];
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
HAL_GPIO_Init(BUTTON_PORT[Button], &GPIO_InitStruct);
/* Enable and set Button EXTI Interrupt to the lowest priority */
HAL_NVIC_SetPriority((IRQn_Type)(BUTTON_IRQn[Button]), 0x0F, 0x00);
HAL_NVIC_EnableIRQ((IRQn_Type)(BUTTON_IRQn[Button]));
}
}